Part Number: AM625 Other Parts Discussed in Thread: TMP100 , AUDIO-AM62D-EVM , SK-AM62A-LP , SK-AM62B-P1 , SK-AM62-LP , SK-AM62P-LP , TMDS62LEVM , TMDS64EVM
TMP100 is an I2C/SMBus interfaced digital temperature sensor that is available on the EVMs…
Part Number: MSPM33C321A Other Parts Discussed in Thread: SYSCONFIG ,
1. Background
Since the LP-MSPM33C321 features an onboard OLED display, you can display images and animations, such as in [FAQ] MSPM33C321A: How to play video 'bad apple' at LP…
Part Number: AM6442 Other Parts Discussed in Thread: TMDS64EVM
The FAQ lists steps on how to build, flash, and boot linux from GPMC-NAND on TMDS64EVM [1] and [2] with AM64x Linux SDK 12.1.0.5.3 [3] + the attached u-boot and kernel patches. [1]. TMDS64EVM…
Part Number: BQ25853EVM Other Parts Discussed in Thread: BQ25853-Q1 , BQSTUDIO
Hello,
Here is a link to the BQ25853-Q1 BQZ file: Charger_1_00-bq25853.bqz
To install this bqz file, download the file and move it to the config folder of the BQStudio…
Part Number: TPS546E25
TPS546E25 Checksum has Different after Importing Script
I export a script with checksum, but when I import into another device the checksum is not the same.
Part Number: TPS7H2201-SEP Other Parts Discussed in Thread: TPS7H2201EVM
Hello,
On both units VIN measures as a short to GND, while VOUT is clean to both VIN and GND. The second unit has degraded progressively and now draws around 700 mA at VIN with…
Part Number: AM2611-Q1
Hello expert,
How should persistent data like filesystems, logs, etc. be handled during a FOTA update.
If the full memory is divided into 2 banks, this would mean after every update, the device will need to copy the persistent…
Part Number: BQ25790 Other Parts Discussed in Thread: BQ25798
With charge enabled (i.e. /CE pin=0 and no TS pin fault), the BQ25790 assumes a discharged battery pack is connected and attempts to close the pack protector for 1.5s by regulating BAT to…
Part Number: TMS570LC4357
Few customers noticied that EXTRST flag is not setting in HDK boards for Watchdog / Software resets, because of this only partial initializations are happenning in startup code and eventually that creating aborts in code execution…