Part Number: MSPM33C321A
The idea here is to reset and re-init the I2C module.
Please find the example as following.
Demo_i2c_target_to_controller_rw_multibyte_fifo_poll_LP_MSPM33C321A_nortos_ticlang.zip
Part Number: TDA4VH-Q1
I'm looking for detailed information on what memories each PBIST instance performs positive and negative selftest on. All instances don't have same kind of memories. So, I would like to understand what each instance specifically…
Other Parts Discussed in Thread: SN6505A-Q1 , SN6501-Q1 , SN6507 , SN6505A , SN6505B , SN6505B-Q1 , SN6507-Q1 , SN6501 , SN6505D-Q1 SN650xx Family – Frequently Asked Questions (FAQ)
This home page is for common questions in relation to the SN6501…
Common Questions
[FAQ] Does TI have crosses for Cirrus Logic recent EOL or discontinued devices like CS536x ADC, CS43x5 DAC, WM8985/CS4243x Codec, CS842x SRC, and CS35L0x amplifiers?
[FAQ] What are some new & exciting parts that TI offers?
…
Part Number: AM13E23019
What are the most Common ADC Terms and their definitions?
What operations can be performed in the ADC Post-Processing Block in hardware?
What is the temperature range of operation for the ADC peripheral?
What is the ENOB…
Part Number: PGA970
I am using PGA970, and I am trying to enable the waveform generator. I'm not seeing anything on the output. Is there a specific register I need to write? Do I need to write firmware to the PGA970?
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: DRA821 , TDA4VM , DRA829 , TDA4VL , TDA4VH
What devices within the Jacinto family support interfacing with UFS devices?
[FAQ] TAS2563: Adjusting Digital Volume Control using I2C
[FAQ] TAS2563, TAS2562, TAS2557, TAS2770 Android/Linux Drivers Link
[FAQ] TAS2563: PDM Interface
[FAQ] TAS2563: What are the .ftcfg, .cfg, .h, .json, and .bin files used for in End System…
[FAQ] DRV2625: DRV2624EVM and DRV2625EVM Windows 10 Driver
[FAQ] DRV26xx Actuators Selection
[FAQ] DRV2605: Closed and Open Loop Description and Examples
[FAQ] DRV2624: Driving Capabilities of DRV2624 & DRV2625
[FAQ] DRV2624: Principals and Method…