Part Number: AM13E232N9
3 devices were connected and sdk dc sync example from the sdk was run .
Sync 1 signals were measured ( PD5 pin) since sync 0 pin is not out on launchpad.
Cycle Time Configured in Twincat
Screenshot…
Part Number: AM13E232N9
The SDK pdi_test example initializes the ESC but does not include PHY register read/write APIs. This FAQ explains how the PHY is accessed and gives the code to add to the example.
(Note: In early Bluewired version…
Part Number: F29H850TU
Q1: How do I configure IDRESPONDERTASKBYTE and RXIDMASK for single IDs, grouped IDs, or all IDs (HGENCTRL = 1)? Q2: How do RXIDMASK and IDBYTE work when HGENCTRL = 0? Q3: How does TXIDMASK relate to RXIDMASK? Q4: Why does RXIDMASK…
Part Number: F29H859TU-Q1
How do I make it so that my application binary and the SBL share a single certificate which will be validated by the HSM ROM, removing the need to authenticate it separately?
How to combine the certification of SBL with a…
Part Number: F29H859TU-Q1 Other Parts Discussed in Thread: SYSCONFIG
The multi-core project can run normally in HS-FS device, the CPU3 can be boot successfully.
But now if I run the multi-core project in HS-SE device, the CPU3 can't boot, CPU1 will…
Part Number: AM62A7
I am using AM6x or TDA4x family of devices. The TRM interrupt table shows a different interrupt number than whats provided in the device tree for my device. Why is that the case?
Part Number: AM2754-Q1 Other Parts Discussed in Thread: AM62P , SYSCONFIG , AUDIO-AM275-EVM
Sitara Audio: Where can I find audio software debugging guides and example codes for McASP and audio applications, apart from what is included in the MCU+ SDK…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG
AM275x: How to use 32-bit audio on McASP with the AASRC , which supports only up to 24-bit samples?
The default aasrc_multichannel_playback example of the AM275x SDK is configured for…
Part Number: AM2754-Q1
How to handle loss and recovery of an external McASP clock (for example A2B) when the McASP Rx feeds an AASRC, without a DSP reset?
In my system one McASP receives audio on an external clock (for example from an A2B transceiver…