Part Number: TDA4VL-Q1
What are the different callback functions in the ECC test framework in SDL?
What is SDL_ECC_ESMCallBackFunction and when is it called?
What is SDL_ESM_applicationCallbackFunction and when is it called?
What is SDL_ECC_applicationCallbackFunction…
Part Number: AM2634-Q1
LWIP enabled devices can get IP address from DHCP server based on host name. To enable this feature on LWIP stack, certain configuration needs to be done.
- Let us pick the enet_cpsw_tcpserver example to enable this feature…
Part Number: AM263P4
Ethernet packets can be blocked or forwarded based on their packet addresses. Unicast address is a specific type of address that is intended for one to one communication.
ALE in CPSW susbystem can be configured to drop packets…
Part Number: AM2634-Q1 Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH
This FAQ highlights how you make a datastructure to be stored in flash in AM263 microcontroller.
Typically we can do this in AM263Px and AM261x microcontroller where XIP…
Part Number: AM263P4-Q1 Other Parts Discussed in Thread: UNIFLASH
This FAQ explains how to setup the flash utility to flash into external flashes which are not supported out of the box. The method mentioned in this FAQ would be the same for AM261 and…
Part Number: TDA4VH-Q1
How to enable the constant monitoing of the linux and remotecores of main domain from mcu domain core (mcu1_0)?
If core is crashed and detetion is done by monitoring, how to enable autonomous recovery?
Part Number: TDP2004
This Master FAQ lists serves as a point of reference to find all FAQs made by TI's signal conditioning Team.
DPHY: 1. [FAQ] SN75DPHY440SS: Is it okay to swap the polarity and lane order? - Interface forum - Interface - TI E2E…
Part Number: AM625
What this FAQ covers? This FAQ demonstrates how to boot Linux on the AM62x SK EVM with 256 MB of DDR instead of the default 2 GB. It provides the complete set of firmware, bootloader, device tree, and kernel changes required.
Part Number: MSPM0-SDK
This thread is used to update the software or hardware update for application note of Single Phase AC Power Monitor with MSPM0
Hardware_Software.zip
Other Parts Discussed in Thread: C2000WARE , SYSCONFIG
This post is meant to specify erratas /document any refinements or clarifications discovered after the C2000Ware release.
Sysconfig migration/Switch feature in Sysconfig 1.26 does not work with…