Part Number: REF5050
Team,
I am trying to find out the differences between the DNC pins (1 and 8) and the NC pin (7).
- Are DNC used for testing/calibration during production? So they are connected to the die and therefore should be left unconnected…
FAQ: Logic and Voltage Translation > Quality and Manufacturing >> Current FAQ
It's extremely common to need to know if one device can be directly replaced with another.
With Standard Logic devices, this is generally an easy process.
The part number…
Part Number: MSP430I2020 Other Parts Discussed in Thread: MSP-TS430RHB32A
Tool/software: TI C/C++ Compiler
Test condition:
- MSP-TS430RHB32A board
- GAIN 1
- Measuring result = 10 data average
- sample program "sd24_ex4_singleConversionSingleChannelPolling…
Other Parts Discussed in Thread: TAS5766M , TAS5768M What you need to develop TAS576xM-based Smart Amp systems
Applies to:
TAS5766M TAS5768M
To start Smart Amp development, you will need to:
1. Request Hardware and Software
a. The Learning…
PurePath Console Motherboard
Wiki entries for PurePath Console Motherboard (aka PPCMB)
http://www.ti.com/tool/purepath-cmbevm
How to configure PPCMB for external audio interfaces
The PurePath Console motherboard can be configured to accept…
Part Number: PGA4311 PGA4311 EVM GUI Problem
Hi, I have a customer who is trying to get the PGA4311 EVM to work and keeps getting an error message.
When I try to set up this EVM on a Win XP system (using sboc277a), i get the following errors too…
Other Parts Discussed in Thread: RC4580 , LM833 "Balanced" Mic Pre-Amplifier (PGA2500/INA166?)
Q:
1. Can "bipolar" input and "balanced" be thought of as the same thing?
2. What follow up will I need to narrow down which pre amp is best?
A: …
Other Parts Discussed in Thread: LM1876 , LM4935 , OPA1662 , OPA1664 Blast from the Past! 1980 NSC Audio/Radio Handbook!
Howdy,
We've gotten several requests for this, so here it is!
Sorry the scan isn't 100% clear, but the print quality of the…
Other Parts Discussed in Thread: TAS5768M , TAS5766M , TAS5756M , TAS5782M Tool/software: Linux
Linux Driver for TAS5766M and TAS5768M
Below is a Linux ALSA driver for TAS5766M and TAS5768M. This driver is kept as simple as possible. Its major purpose…
How to revive a MC57xxPSIA board
The MC57xxPSIA is a board used to interface, configure and control the TAS57xx family of digital audio amplifiers.
The Firmware of the MC57xxPSIA may get corrupted, resulting in Windows not recognizing the board…