Part Number: AM6442
The MPU ARMv7 flash region must be configured with appropriate memory attributes and access permissions to enable flash write operations. Incorrect configurations such as read-only permissions, misaligned region boundaries, or improper…
Part Number: F29H850TU Other Parts Discussed in Thread: SYSCONFIG
Is there any document explaining CAN module configuration parameters and how to configure these parameters in Sysconfig tool?
Part Number: TPS546E25
How to Change TPS546E25 PMB_ADDR (0xD3) on a Secondary Device in a 2-Phase Configuration
There are multiple devices on the serial bus and need to change the address from the default pin strap address to avoid conflict
Part Number: AM62P
K3 SoC (AM64x, AM62x...) have a set of One-Time Programmable (OTP) efuses which is anchoring Root-of-Trust (RoT) secure boot chain. Linux SDK supports the RSA key signed secure boot [1]. The FAQ discuss how to enable ECDSA key signed…
Part Number: MSPM0G3507
Use function of DL_Interrupt_registerInterrupt to define all the interrupts that used.(This function will copy the vector table into SRAM then modify the interrupt offset address and modify the interrupt ISR entry address as…
Part Number: MSPM0G3507
Use function of DL_Interrupt_registerInterrupt to define all the interrupts that used.(This function will copy the vectory table into SRAM and modify the interrupt ISR entry address as needed)
Example:
DL_Interrupt_registerInterrupt…
Part Number: PGA900 Other Parts Discussed in Thread: UNIFLASH
I am trying to flash firmware to PGA900/970, and I am getting a data verification error. I have verified my hardware connection.