Part Number: AM2634-Q1 Other Parts Discussed in Thread: UNIFLASH
Hi Expert,
I'm experiencing long delays when loading images into external flash using UniFlash. The tool spends the majority of its execution time initializing and setting up the environment…
Part Number: AM625 Other Parts Discussed in Thread: TMP100 , AUDIO-AM62D-EVM , SK-AM62A-LP , SK-AM62B-P1 , SK-AM62-LP , SK-AM62P-LP , TMDS62LEVM , TMDS64EVM
TMP100 is an I2C/SMBus interfaced digital temperature sensor that is available on the EVMs…
Part Number: MSPM33C321A Other Parts Discussed in Thread: SYSCONFIG
1. Background
Since the LP-MSPM33C321 features an onboard OLED display, you can display images and animations, such as in [FAQ] MSPM33C321A: How to play video 'bad apple' at LP…
Part Number: AM6442 Other Parts Discussed in Thread: TMDS64EVM
The FAQ lists steps on how to build, flash, and boot linux from GPMC-NAND on TMDS64EVM [1] and [2] with AM64x Linux SDK 12.1.0.5.3 [3] + the attached u-boot and kernel patches. [1]. TMDS64EVM…
Part Number: BQ25853EVM Other Parts Discussed in Thread: BQ25853-Q1 , BQSTUDIO
Hello,
Here is a link to the BQ25853-Q1 BQZ file: Charger_1_00-bq25853.bqz
To install this bqz file, download the file and move it to the config folder of the BQStudio…
Part Number: TPS546E25
TPS546E25 Checksum has Different after Importing Script
I export a script with checksum, but when I import into another device the checksum is not the same.
Part Number: TPS7H2201-SEP Other Parts Discussed in Thread: TPS7H2201EVM
Hello,
On both units VIN measures as a short to GND, while VOUT is clean to both VIN and GND. The second unit has degraded progressively and now draws around 700 mA at VIN with…
Part Number: AM2611-Q1
Hello expert,
How should persistent data like filesystems, logs, etc. be handled during a FOTA update.
If the full memory is divided into 2 banks, this would mean after every update, the device will need to copy the persistent…
Part Number: BQ25790 Other Parts Discussed in Thread: BQ25798
With charge enabled (i.e. /CE pin=0 and no TS pin fault), the BQ25790 assumes a discharged battery pack is connected and attempts to close the pack protector for 1.5s by regulating BAT to…