Part Number: IWR6843AOPEVM Other Parts Discussed in Thread: MMWAVE-SDK , IWR6843AOP , IWR6843 ,
MMWAVE-SDK 3.2.x startup sequence needs to be updated for IWR6843 ES1.0 and IWR6843AOP ES1.0 devices
NOTE: The following update will be included in future…
Part Number: TAS2505
Hi,
I would like to gather up some information about this device protection in one place. Our TAS2505 and TAS2505-Q1 devices feature protection scheme against situations like:
Overcurrent / Short Circuit
Class-D driver…
I have installed SimpleLink SDK 3.30 (or any other SDK version that requires the IAR EW for Arm 8.32) and now I see the warning “SYS/BIOS ROV session manager failed - can't find a JVM” whenever I start the debugger. I also don't have the menu TI-RTOS…
Other Parts Discussed in Thread: ENERGYTRACE Tool/software: Code Composer Studio I keep getting "com/ti/dvt/energytrace" errors when I start up CCS. How do I resolve this?
Other Parts Discussed in Thread: TI-RTOS-MCU I want to create an application using the TI-RTOS kernel (SYS/BIOS). What options do I have to create kernel objects?
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 , COEFFICIENT-CALC
Hi,
Our TAS2505 and TAS2505-Q1 devices feature up to six programmable biquads that can be used to add some equalization to your application. The GUI for this device…
Other Parts Discussed in Thread: DRV2700 , DRV8662 Hi,
When using a haptics driver device from the DRV26xx, DRV2700 and DRV8662 families, there are many questions around the actuator to be used. As general information, we can get some details about…
I'm using Runtime Object View (ROV) and I see the following:
Is this a problem or expected behavior? Can you please give more details?
Note: the same is show in ROV Classic.