Part Number: LM5114 Other Parts Discussed in Thread: LMG1020
What is the maximum operating frequency of this gate driver (LM5114BMF/NOPB)? I would like 24 MHz.
Maximum operating/switching frequency of a gate driver depends on many factors including…
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Some of the TI translators have requirements during normal operation mode to have Vcca <= Vccb ( TXS/ TXB01xx) or Vrefb>= VrefA+0.8V(LSF). However, the TI translation devices do…
FAQ: Logic and Voltage Translation > Logic Technology >> Current FAQ
The I OFF specification guarantees the I/O ports are in high impedance whenever either one of the power supply is at pulled to ground (0V) or close to gnd(<100mV as specified for the…
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
For the TXB family, unused I/O ports are recommended to be tied to GND through a weak pulldown resistors (>=100kohm).
For TXS devices, the internal 10kohm pull-ups resistors will…
Part Number: CC2652R Other Parts Discussed in Thread: Z-STACK , SIMPLELINK-CC13X2-26X2-SDK , CC1312R , CC1352R , , CC2642R
Hello All,
Z-Stack Core v1.0.0.0, part of Z-Stack 3.3.1 as included in the SimpleLink™ CC13x2 / CC26x2 SDK v3.10, has been certified…
Part Number: BQ24040 Other Parts Discussed in Thread: BQ24090 , BQ21040 , BQ24050
Hello Team
I have completed my design and layout can someone review it for me?