Part Number: LP5814 Other Parts Discussed in Thread: LP5816 , LP5817 , LP5815
Tool/software:
Four steps to solve the I2C NACK,
Hardware check
Device I2C slave address check
Real output I2C data bits check
SCL / SDA high low level check …
Part Number: TDA4VE-Q1 Tool/software: How can we read Control registers of c7x from an application. Including registers such as IEAR and IERR to monitor error.
Part Number: TMS320F28388D Tool/software:
Details:
A Cortex-M4 corner case condition, where it terminates stalled AHB transaction before completion, aligned with a specific access sequence, will cause CM interconnect and CM flash wrapper to go out…
Part Number: TDA4VH-Q1 Tool/software: Hi Team,
How can I optimize DSPLIB_add_example.cpp code to reach the performance levels mentioned in the datasheet summary ?
Part Number: AM625 Other Parts Discussed in Thread: BQ32000 , AM62A7 , AM62A3 , SYSCONFIG , , AM62P , AM62L ,
Tool/software:
Hi TI experts,
I see that there is a RTC module instance.
Do you have any guidance on the usage of the RTC
FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ
The maximum trace length that ground-level translators (as well as logic devices) can drive is 60 mm. This is a safe trace length for most devices to drive across the majority…
FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ
To use the ground shift capability, voltage supplies need to be isolated and fall within the recommended operating conditions.
Let’s use the figure above as an example…
Other Parts Discussed in Thread: TXG8041
FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ
A negative signal can be generated from ground-level translators as long as the user’s system has a negative supply rail. To prevent…
FAQ: Logic and Voltage Translation > > Current FAQ
[FAQ] What are the differences between Ground-Level Translators and Digital Isolators?
[FAQ] Can I generate a negative PWM signal from a positive PWM signal?
[FAQ] Is DC ground shifting possible…