Part Number: MCU-PLUS-SDK-AM261X Other Parts Discussed in Thread: LP-AM261 , SYSCONFIG Tool/software: Hi TI experts,
All ADC2 values output as '0' on AM261x.
Example output on is adc_multiple_soc_epwm_am261x-lp_r5fss0-0_nortos_ti-arm-clang and on…
Part Number: AM2612 Tool/software: Hi TI experts,
I am using the AM261x-LP board and running into the following USB issues:
I tried running the SBL DFU application via the dfu-util tool provided. I am not able to get the device to enumerate after…
Part Number: UCC27714
Tool/software:
There are numerous 600V half-bridge gate drivers available in 8 pin SOIC packages and also higher pin count 14 pin packages. With the 8 pin SOIC package, only the basic half-bridge gate driver functions are available…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TDA4VH , J784S4XEVM Tool/software: I'm seeing issues with the display experiencing sync losts when running the TIDL AVP demo. How do I balance the transaction loads and priorities so that the DSS…
Part Number: PROCESSOR-SDK-AM62X
Tool/software:
Greetings,
When working with a flash part like S25HL512T or S28HS512T , one will come across Uniform vs Hybrid mode.
The points which this FAQ covers is:
What is Uniform vs Hybrid Mode for the…
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: AM62P , SK-AM62P-LP , PROCESSOR-SDK-AM62A
Tool/software:
Hi, For my application, I don't need PD controller for power negotiation. But in SK-AM62A-LP design, PD controller is also used for…
Part Number: TDA4VM
Tool/software:
ETHFW returns error while registration of same MAC address with different VLAN from same client. This issue is observed on 10.1 TI SDK.
Part Number: MCU-PLUS-SDK-AM261X Tool/software: Hi TI experts,
I am unable to import Networking (Enet CPSW) examples in CCS workspace from the AM261x MCU+ SDK.
Part Number: MCU-PLUS-SDK-AM261X Tool/software: Hi TI experts,
I am unable to find ethernet networking (enet cpsw) examples in the MCU+ SDK for AM261x. For AM263x and AM263Px, I am able to locate the examples inside the <mcu_plus_sdk>/examples/networking…