[FAQ] TAS2563: Adjusting Digital Volume Control using I2C
[FAQ] TAS2563, TAS2562, TAS2557, TAS2770 Android/Linux Drivers Link
[FAQ] TAS2563: PDM Interface
[FAQ] TAS2563: What are the .ftcfg, .cfg, .h, .json, and .bin files used for in End System…
[FAQ] DRV2625: DRV2624EVM and DRV2625EVM Windows 10 Driver
[FAQ] DRV26xx Actuators Selection
[FAQ] DRV2605: Closed and Open Loop Description and Examples
[FAQ] DRV2624: Driving Capabilities of DRV2624 & DRV2625
[FAQ] DRV2624: Principals and Method…
Part Number: AM13E23019 Other Parts Discussed in Thread: SYSCONFIG
Hi experts,
I am using the AM13E230x device along with the mcu_sdk v26.0
Is it possible to enable a custom bootloader in TI AM13E230x?
If so, how to enable and flash the custom…
Part Number: TPS546E25
When I write to VOUT_COMMAND (0x21) on TPS546E25, the VBOOT_OFFSET (0xD5) does not change.
When write to VOUT_COMMAND (0x21), VOUT_COMMAND does not cause VBOOT_OFFSET (0xD5) to change,
The tables below highlight the working configurations of custom OSPI and QSPI serial NOR/NAND Flash Parts
Note: After using the values for the Flash part present in the below tables, run the OSPI Flash IO example to verify if Flash operations are working…
Part Number: AM2434 Other Parts Discussed in Thread: UNIFLASH , SYSCONFIG
uart_uniflash.py allows to flash binaries to the flash on a EVM. UART is used as the transport or interface to send the file to flash to the EVM. When the uart_uniflash.py script…
Part Number: AM2434
Facing issues while running the loadJSFile command from the CCS scripting console.
Please refer image below.
I am using the CCS v20.4.0.