Part Number: PGA970
I am using PGA970, and I am trying to enable the waveform generator. I'm not seeing anything on the output. Is there a specific register I need to write? Do I need to write firmware to the PGA970?
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: DRA821 , TDA4VM , DRA829 , TDA4VL , TDA4VH
What devices within the Jacinto family support interfacing with UFS devices?
[FAQ] TAS2563: Adjusting Digital Volume Control using I2C
[FAQ] TAS2563, TAS2562, TAS2557, TAS2770 Android/Linux Drivers Link
[FAQ] TAS2563: PDM Interface
[FAQ] TAS2563: What are the .ftcfg, .cfg, .h, .json, and .bin files used for in End System…
[FAQ] DRV2625: DRV2624EVM and DRV2625EVM Windows 10 Driver
[FAQ] DRV26xx Actuators Selection
[FAQ] DRV2605: Closed and Open Loop Description and Examples
[FAQ] DRV2624: Driving Capabilities of DRV2624 & DRV2625
[FAQ] DRV2624: Principals and Method…
Part Number: AM13E23019 Other Parts Discussed in Thread: SYSCONFIG
Hi experts,
I am using the AM13E230x device along with the mcu_sdk v26.0
Is it possible to enable a custom bootloader in TI AM13E230x?
If so, how to enable and flash the custom…
Part Number: TPS546E25
When I write to VOUT_COMMAND (0x21) on TPS546E25, the VBOOT_OFFSET (0xD5) does not change.
When write to VOUT_COMMAND (0x21), VOUT_COMMAND does not cause VBOOT_OFFSET (0xD5) to change,