Part Number: AM2612
Announcement: Zephyr RTOS Pre-release available on the AM261x SoC!
We’re excited to announce that preliminary support for Zephyr RTOS is now available on the AM261x microcontroller. This integration unlocks a modern, highly scalable…
Part Number: AM2612 Other Parts Discussed in Thread: UNIFLASH
Step-by-Step Guide to running profinet example on LP-AM261x.
Requirements:
1. I ND COMMS SDK
2. CCS
3. Compiler
4. Syscfg
5. Uniflash GUI
6. Python and OpenSSL
7. LP-AM261x…
Part Number: UCC5881-Q1 Other Parts Discussed in Thread: STRIKE
The UCC5881-Q1 offers enhanced flexibility in DESAT settings through its SPI interface, allowing you to easily adapt your control board to different power modules (such as IGBT or SiC…
Part Number: UCC5881-Q1 Other Parts Discussed in Thread: UCC5880-Q1 ,
If you're planning to upgrade your design from UCC5880-Q1 to UCC5881-Q1, there are several key factors to consider. It’s easy to upgrade since both devices have pin-to-pin compatibility…
Part Number: UCC5881-Q1 Other Parts Discussed in Thread: UCC5880-Q1 ,
UCC5881-Q1 is TI’s latest programmable isolated gate driver, offering pin-to-pin compatibility with the exact same package and pinout as UCC5880-Q1. This enables designers to keep…
Part Number: AM2612
Hi ASM team,
I get the following error after trying to build a simple GPIO toggle program on a clean install of the 10_02_00_15 SDK. Have we seen this before?
All the best,
Ethan Cope
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG , TAD5212
Mcasp buffer order
To be short, in case of multiple serializers used in one Mcasp, the samples are placed interleaved by slot not frame by default. (Please check the "12.1…
Part Number: J722SXH01EVM
Tool/software:
How do I use the Fusion2 board with the J722SXH01EVM ?
When I try to run the single camera demo, I see the following error:
[MCU2_0] 76.844004 s: Error writing 0x01 to de-serializer(0x3d) register 0x4c…
Part Number: MSPM33C321A
Tool/software:
When MSPM33 enter a state where CCS is unable to connect to M33 core, follow the below procedure to implement Factory Reset.
CCS version >= CCS v 20.4.0.5
Step 1 - Launch project less debug
Step 2 -…