Part Number: MSPM33C321A Tool/software: 1. Background
If there is a display, then you can use it to play 'bad apple'
Now MSPM33 Launchpad has a 128*32 OLED on the board...
2. Demo video:
3. Required hardware/software
Hardware
LP-MSPM33C321A…
Part Number: CC2745R10-Q1 Tool/software: Issue:
When trying to flash or debug a CC27XX using CCS 20.3.0, the following error is reported:
Cortex_M33_0: Flash loader: CC23xx_CC27xx_FLASH_LIBRARY_VERSION 4.1.0.141
GEL: Error while executing OnPreTargetConnect…
Part Number: TDA4VM Other Parts Discussed in Thread: SYSCONFIG , TDA4VH-Q1 Tool/software: What is the K3 Resource Partitioning tool? What is it useful for within my application? How do I use it?
Part Number: MSPM0C1104 Tool/software: Here provide an script to do factory reset with J-Link, there is an readme file to show you how to do it. Important thing is remember to modify the device in open factory_reset.bat and connect the reset pin with…
Part Number: AUDIO-AM275-EVM Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH
Tool/software:
Background
Current SDK supports boot images of multiple cores being combined to one image in mcelf format. This guide explains how is multicore images…
Part Number: TDA4VM
Tool/software:
The EthFW 11.1 release has an interface change that breaks the ABI with 11.0 or earlier versions of the QNX io-sock thin-client driver. For the driver to work correctly, an update to the ABI interface header file…
Part Number: TMS320F28P550SJ Other Parts Discussed in Thread: C2000WARE Tool/software: Hello,
I am facing an issue where in my program builds succesfully however, when I try to flash it/ launch a debug session, I get the following error.
After flashing…