Part Number: MSPM0C1104 Tool/software: This is the software resources used in the application note: Cooling FAN Controller with MSPM0
MSPM0 Cooling Fan Controller Demo.zip
Part Number: MSPM0G3507
Tool/software:
This is the software resources used in the application note: MSPM0 LFU Bootloader Implementation
https://www.ti.com/lit/an/slaae88c/slaae88c.pdf
MSPM0 LFU Bootloader Implementation release v1.4.zip
File…
[Click here to return to homepage]
MSPM0 HARDWARE DEVELOPMENT
Listed below are a variety of documents and FAQs to assist with the physical implementation of MSPM0 devices
Layout and Design Tips
(Hardware development guidance, passive layout…
Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: AM62P
Tool/software:
Hello, I'm using AM62x/AM62A/AM62P and I want to set a GPIO high or low during the R5 SPL.
If you are interested in doing this in U-Boot command line, follow…
Part Number: MOTORSTUDIO
Tool/software:
Steps to resolve the above error: " Error while installing vcp driver ":
If MOTORSTUDIO is already installed in the computer and the above error message is displayed, uninstall MOTORSTUDIO from the computer…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I have a flash device that is different from the one being used in the Audio EVM and also non-existent in the SysConfig tool. How do I know if this device will work with…
Part Number: AM62L Other Parts Discussed in Thread: TMDS62LEVM
Tool/software:
Hi TI Experts,
I am working on custom board design and have query on the below:
Available design files and supported CAD tools.
I am specifically interested in knowing…
Part Number: AM6422
Tool/software:
Hi.
MMCSD1:
Is there an option to select between different driver strength for:
a) 3.3V signaling
b) 1V8 (UHS-I) signaling
The "MMCSD1_CAPABILITIES" Register indicating that Driver Type A,C and D are…
Part Number: BQ41Z50
Tool/software:
To use the ECC Authentication tool for BQ41z50, refer to the provided PDF guide. It offers a high-level overview of the ECC algorithm and step-by-step instructions for using the ECC GUI. PDF Guide and Executable…