Part Number: AM62A1-Q1 Other Parts Discussed in Thread: AM62A7 , AM62A3 , AM62A7-Q1 , AM62A3-Q1 , , SYSCONFIG , SK-AM62A-LP , AM62D-Q1
Hi TI Experts,
I am starting a new project and want to use Sitara AM62Ax processor family in the design. Can you…
FAQ: Logic and Voltage Translation > Power and Thermals >> Current FAQ
We have been updating the thermal values in our datasheet, so you may have received a notification about datasheet changes to the thermal values or noticed a datasheet revision about…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VM
We are currently working on the TDA4VM platform , and the user application rpmsg_char_simple runs as expected when initiated from the A72 side .
However, we are facing an issue while trying…
Part Number: BQ25188
The BQ2518x resets its R/W registers to the default values whenever a reset condition occurs. This can happen due to watchdog timers, power-on reset (POR), or a software-initiated reset.
Watchdog timer
The BQ2518x includes a…
Part Number: BQ25188
Power Dissipation
The BQ2518x is a linear charger with power path. Power path is a feature that allows the BQ2518x to power the system from the input source while simultaneously charging the battery. The back-to-back input FETs…
Part Number: AM275-FREERTOS-SDK
The FreeRTOS SDK and MCUPlus SDKs both contain additional libraries, such as DSPLib. These libraries by default are not meant to run within CCS projects directly, but rather to be compiled with cmake.
It is possible…
Part Number: AM625
BINMAN tool is currently used to sign u-boot binary in Linux SDK, where the signing key is locatable under Linux SDK folder. There's a need to use the signing key stored in the external secure key server when switching to the production…
Part Number: TDA4AEN-Q1
Example explaining the steps of combined app image with WKUP R5F and MCU R5F in J722S without HLOS
https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-j722s/latest/exports/docs/mcu_plus_sdk_j722s_11_01_00_15/docs/api_guide_j722s…
Part Number: TDA4VH
Support for user-mode host-id for A72/A53 HLOS running user-mode drivers: ==============================================================
Before the SDK 11.2 release, the UDMA resource allocation utilized elevated privileges for…