Part Number: DLP2000
Hello DLP® LightCrafter™ Display 2000 users!
We have recently pushed a new code update to the BeagleBone Black Debian distribution for this EVM. This update provides some reference code and a program to enable structured light…
This document addresses most frequently asked questions fro the LM388X analog sequencer. Pleae read thist first to ensure that you questions are covered before posting.
5164.LM388X Frequently Asked Questions and Answers.pdf
Thanks
Part Number: DLPDLCR2000EVM
All,
When using the DLP LightCrafter Display 2000 EVM, there are some situations where you may want to use the EVM with a system that does not have native support for the EVM's drivers. An example of this is using a custom…
Part Number: PROCESSOR-SDK-TDAX
Dear Developers,
This post provide links to list of Frequently asked questions, Application Note and Other useful links.
Users are request to check FAQ wiki before posting their queries on forum.
FAQ - http…
Watch this TI Precision Labs training video to understand how powered-off protection works with your system.
This tech note has detailed information on powered off protection.
PoweredOffProtection_B.pdf
Why do I need a switch with powered off…
Part Number: TPS65072EVM-430
I would like to purchase TPS65072EVM to get exposure on PMIC .When i am trying to get the user manual of TPS6507X EVM software i could not able to get.And i would like to know what kind of tests i can perform on this EVM…
Part Number: LP8758-E0 Other Parts Discussed in Thread: LP8758
I got the answer that LP8758-E0 Max duty is 100% from the following URL E2E post.
However there is "dropout voltage" (min 0.7V) on datasheet electrical characteristics.
What does this…
Part Number: TPS65070
I'm using the TPS65070 as Power-Manager of an IIoT-System. As power-supply I use LiPo or/and AC. After booting the TSP EN_DCDC1 is high and in the CON_CTRL1-Register there is the default setting “01111111” This means after pulling…
Part Number: ADS1282
Hi all,
For unipolar mode (AVDD=5V, AVSS=0V, VREFP=5V, VREFN=0V), ADS1282 full-scale input voltage is from 0V to 2.5V. Am i right?
Also data code is range from 00000000h to 7FFFFFFFh for FIR filter. Am i right?
Most of…
Part Number: TIDM-THREEPHASEMETER-F6779 Other Parts Discussed in Thread: MSP430F6779
With Reference to the reference design:
SLAA577G–January 2013–Revised August 2015 Implementation of a Three-Phase Electronic Watt-Hour Meter Using the MSP430F677x…