Hi Deexith,
I'm sorry I made a mistake, this step really didn't increase the 2Dfft noise, but I think there will be a change in the distance dimension at zero velocity. It's uncertain if this could cause other problems.
The radar is mounted…
Part Number: TPS546D24A Tool/software: Hi TI Team,
We are using power converter MPN: TPS546D24ARVFR in our new project. Please verify the attached files and let us know the feedback.
Voltage
Voltage ripple
Current consumption
Step Current …
Part Number: MSP430F122 Tool/software: FCT test failure , Due to the same adverse phenomenon, J3 voltage is too low, Defective rate: 12%
After analysis and verification, it has been preliminarily confirmed that IC U5 has poor functionality
1. Heating…
Hello,
I have dumped register on custom board , it is not as expected:
It has value 24, meaning MCU_BOOTMODE3 pin is not as expected.
I can do same on the TI EVM, to confirm if it is HW switch issue or SW..
Best regards,
Milena
Hi,
In the ecc_func_app present in SDL, t o test the inaccessible RAM IDs, an error is injected by SDL, but since there is no direct way to access the memory, the error interrupt is forced by manipulating the ECC’s interrupt status registers. For information…
Hi Sudheer, The phy-mode is rgmii-rxid P: /devices/platform/bus@100000/bus@100000:bus@28380000/46000000.ethernet/net/eth0
M: eth0
R: 0
U: net
I: 2
E: DEVPATH=/devices/platform/bus@100000/bus@100000:bus@28380000/46000000.ethernet/net/eth0
E: SUBSYSTEM…
Part Number: AM3354
Tool/software:
Linux SDK 02.00.02.11
As the title: Weston and Matrix start up normally, but the screen only displays blue. #1、run /etc/init.d/weston start , and the screen turns blue
/var/log/weston.log
Date: 2024-12-13 UTC
[14:51…
Hi Brandon,
It may be similar question, pls refer to e2e.ti.com/.../3075201
Could you try with the TPS65400-GUI? You can find it under its product folder.
Besides, you may need another firmware version in your USB2ANY, please try below one,
0167.USB2ANY_1_19_0_0…