Part Number: 2N7001T-Q1 Other Parts Discussed in Thread: 2N7001T Hi Team,
Is there an alternative source you would recommend to the 2N7001TQDCKRQ1 to second source ourselves from a TI perspective? Device would need to be pin-to-pin, but does not have…
Part Number: 2N7001T I am designing 2N7001T with 1.8V system. I have 2 voltage sources of 1.8V. Can IC 2N7001T be used with both VCCA and VCCB of 1.8V.
in datasheet it is mentioned that we can use this IC for up or down voltage translation.
Part Number: 2N7001T Tool/software: Hi,
We have used a 2N7001T 3.3V to 2.5V clock translator on one of our recent prototypes. Due to the high radiated emissions measured in the near-field, compared to a previous board revision not using this component…
Part Number: 2N7001T We would like to use the part in the following manner:
Va=1.8V with the option of using a 1.8V or 3.3V input
Vb would be 3.3V
Is this feasable.
Part Number: 2N7001T
Hello,
We're designing with the 2N7001T and had a question about the "Input Transition Rise or Fall Rate" specified in the datasheet.
section 6.3 lists the "max input transition rise or fall rate" = 100ns/V.
However section…
Part Number: 2N7001T
[Case:709346]Technical Data Inquiry
SiliconExpert is contracted by our customer to work with their suppliers for accuracy and compliance purposes.
As the part "2N7002" is valid on the datasheet " https://download.siliconexpert…
Part Number: 2N7001T-Q1 Tool/software: In my application VCCA = 3.3V and VCCB = 1.8V. Should I use the Ioh and Iol specification for 8mA to determine the min and max voltage output?
The 2N7001T-Q1 datasheet shows Voh and Vol for the different mA loads…
Part Number: 2N7001T What about the current drive output capability at 100Mbps? Is it 50mA at Vccb = 3.3V?
requirements are: 100Mbps (i.e. 10ns minimum pulse widths), 1ns or less rise/fall times, and 50 Ohm drive or at least be able to put out 50mA…
Part Number: 2N7001T
In application report SCEA062A related to 2N7001T. I see some comparations between NMOS level shifter and 2N7001T. When talk about 'Vcc isolation", it says that for NMOS solution, when the power supply is at 0V, the IO pins are…
Part Number: 2N7001T Other Parts Discussed in Thread: SN74LVC1G11 customer reported 2N7001T heat issue.
their user scenario is
VCCA=3.3V, VCCB is 1.8V and 2N7001T input is always "high"..
According to datasheet, the power consumption in 2N7001T…