Thank you Clemens for providing this answer.
Hey Vijay,
Please see the additional resources below for more information:
Voltage Translation Application Quick Reference
Common Risks of Discrete FET Voltage Translation and Advantages of TI’s Integrated…
Part Number: SN74LVC1G126-Q1 Other Parts Discussed in Thread: 2N7001T-Q1 , SN74LVC125A-Q1 , SN74LVC2G125-Q1 Dear logic friends,
Harman has challenges with the speed of a buffer.
Harman is down converting from 3.3V level to 1.8V level at 73MHz
Before Buffer…
Part Number: LSF0204 Other Parts Discussed in Thread: LSF0102 , 2N7001T , SN74AUP1T34 , SN74AUP1G125 , SN74AUC1G125 , TXU0101 , SN74LV1T34 Hi team,
My customer is looking for 13.3V to 1.8V 3-ch level translator which supports I2C and SPDIF.
Does LSF0204 support…
Part Number: TCA5405 Other Parts Discussed in Thread: LSF0101 , 2N7001T , TXU0101 , SN74LVC1G07
Hello E2E Experts,
Good day.
Please share the internal structure of the TCA5405 to understand what should be the value of the pull-down resistor in the attached…
The rise/fall rate is not directly related to the frequency; it describes the slope of the signal edges, not the interval between the edges. If your signal has slower edges, you need to use a different device, probably with Schmitt-trigger inputs.
For…
1. The DP83867IR's MDC pin has an internal pull-down resistor. This does not work with an open-drain translator like the TXS. Better use a fixed-direction translator like the 2N7001T or TXU0101.
2. Yes.
3. This is probably caused by the TXS's edge…
For the clock signal, you could use any fixed-direction or direction-controlled level shifter, e.g., TXU0101, 2N7001T, or SN74LXC1T45/SN74LVC1T45.
Anyway, the TXS has edge accelerators, but otherwise it is a passive switch and has no DC drive strength…