Other Parts Discussed in Thread: TMS570LS3137 , SEGGER , 4213 I was debugging the STC of the TMS570LS3137.And I met a problem that I could not download the program into the flash. I know this chip cannot debug during the STC, but why I cannot write into…
Part Number: DRA750 Other Parts Discussed in Thread: DS92LV2422 , TVP7002 , 4213 Hi ,
This is customer board .The video decoder DS92LV2422 couldn't work with VIN3A port .
I have checked that DS92LV2422 can output RGB data normally ,
It crashes when…
Part Number: ADS1284 Other Parts Discussed in Thread: 4213 , 4428 , 4430 , 4460 The analog input is shorted, but the data looks strange, the offset is very high at the begining, but lower and lower, after about 40 seconds it get back to normal.
Please…
Part Number: AM4376 Hi,
a customer's system is using the AM4376 and Linux 5.4 using a ti-linux-kernel.
We are running into occasional (seemingly random) watchdog resets, but do NOT see dmesg or syslog traces showing what led to the reset. There…
Part Number: TMS320C6678
Hi,
We generated individual interrupts at each GPIO pin. But, We facing the multiple interrupt generation at GPIO pins into a signal. We want to use multiple interrupt generation using the Event Combiner for the GPIOs( into…
Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: BQ34Z110 , BQ34Z100 , 4213 , 4460 , 4430 , 4428 Dear Texas Instrument's Supporter.
My's name is Chien, I have some problems with your BQ34z110 product, The problem's code: The battery capacity…
Hi Vishal
After shifting 6AO.1.1 Android release.we are getting isssues like
1.whole HMI is going freeze in case of playing songs and Navigation in back ground.
Adb logs for your refrence
--------- beginning of system
01-01 00:00:02.916 155…
Part Number: SK-AM62 Other Parts Discussed in Thread: AM625 Hello Sir,
I am trying to boot the SK - AM62x EVM board from eMMC memory.
We are able to boot the board from SD Card.
For the emmc booting: followed these steps in serial prompt after…