Part Number: CD4069UB Other Parts Discussed in Thread: CD40109B i needed to step up the 3.3-volt logic to more than 8 volts. we have CD4069UB ic available with us. when i saw datasheet i could see that by using VDD at 10 or 15 volts. the input PWM can…
Part Number: ADS1293EVM Other Parts Discussed in Thread: ADS1293 , ADS1298 Hi
We have a new project for ECG application for 8-lead.
ADS1293 spec mention two AFE connection in series for 8-lead ECG application.
How could I verify two AFE connection…
Part Number: DRV8884EVM Other Parts Discussed in Thread: DRV8884 , DRV8885 , DRV8886 Hello team,
I got the question from the customer about the DRV8884/5/6 thermal measurement result on EVM.
They measured all that device with the same condition…
Part Number: TLV62585 Hello,
Our customer is planning to evaluate TLV62585PDRL and he has a question about the data sheet efficiency data Figure 5 to Figure 8.
Are these data taken with feed forwad capacitor ? Would ypu be able to disclose the test…
Part Number: ADS1298 My team and I are using two ADS1298s with TQFP packages for an EMG application. All negative differential pins are tied to ground and the ADCs were both soldered by hand.
Our C program (using a pic24fj128ga204 uC) is designed to…
Part Number: CC-ANTENNA-DK2 Hi,
Board #8 does not mention which switch is used (U2). I assume it is the same switch as in board # 5 (PE4259SCBECT-Z). R22 on board #5 is 8.2 kOhm. The equivalent resistor R20 on board #8 is 8.2 Ohm. I assume this is an…
Part Number: 14-24-LOGIC-EVM The pin 1 of CD4071BE through a 10KOHM is connected to "0" gives me 1.44v on pin 1. The measured leakage current to "0" is 120uA. With a 47KOHM pull down resistor on pin one the output stays high at 3.78V.
CD4071BEs are…
Part Number: TMS320F28034 Other Parts Discussed in Thread: C2000WARE Tool/software: Code Composer Studio Hi,
F28034 SCI Communication will lost data when transfer 8 bytes, only 5 bytes can be transfer. but the configuration in F28232 is as the same…
Part Number: AM5728 Tool/software: Linux Hi SIr
We use Processor SDK 5.01 with our customized board for development.
We would like to know how to enable UART port from 1 to 10.
Do you have sample code or document how to modify dts or other necessary…
Hi,
I am dealing with a negative common mode voltage signal path switching problem,
is there any circuit can convert my MCU L/H=0/3.3V control logic to L/H= -3V/0V or -3V/+3V ?
my channel dc voltage to be switched is -1.0V, and the current is 150mA…