Part Number: ACF2101 Tool/software: Hello team,
What do C1 and C2 mean in the chart "total output nose vs C1 and C2" at Page6 in datasheet? If C1 is Sensor capacity Cin and C2 is Externally installed Cintegration, Total Noise value in "total…
Part Number: ACF2101
Why VS1 5V source is connected parallel to VS3 and VS4 in above simulation, that voltage source is not actually connected to any components but why are using.
Part Number: ACF2101 In this Simulation, Why two diodes(D4 1N4148) are connected with current source and also if i simulate without diodes why i am not get simulation result properly.
Part Number: ACF2101 How to know the Microcontroller to enter into Hold mode after Integration mode is done, and then controller don't know when the integration is done (because input square pulse may start at any time, so how to synchronize the input…
Part Number: ACF2101 How to know the square wave signal(in 1pA value) is now come from current source, based on that arm controller can close the hold switch for integration operation on ACF2101.
Part Number: ACF2101 Why in the ACF2101 IC datasheet, in specification the voltage output range, typical value is crossing the Min. & Max. Limit and explain it.
Part Number: ACF2101 Other Parts Discussed in Thread: TINA-TI , IVC102 Hello,
I'm trying to evaluate ACF2101 against the conventional T transimpedance amplifier in terms of noise reduction.
As a first step I'm trying to simulate the ACF2101 in LTspice…
Part Number: ACF2101 Hello Team,
Good day.
My customer is planning to use the ACF2101 and wanted to clarify few things. According to the datasheet the integrator output voltage range is -10V to 0.5V. All of the application examples show input current flowing…
Part Number: ACF2101 As I'm new to this switched capacitor device, I have a question on the APPLICATION BULLETIN SBOA034 ( Comparison of Noise Performance of FET Transimpedence Amp/Switched Integrator from Bonnie Baker).
For the bandwidth optimised…