Part Number: ACF2101
I am trying to use AC2101 to detect very tiny currents using integration times in the 20-second range. So I’m trying to minimize any ground currents finding their way into the signal path.
What is the purpose of the Select switch…
Part Number: ACF2101 Other Parts Discussed in Thread: IVC102 Dear Support,
I am trying to configure the ACF2101 with current input. The power supply of the integrator is -15V, respectively +5V. I have applied a DC current of 0.1uA at the input from…
Part Number: ACF2101 As I'm new to this switched capacitor device, I have a question on the APPLICATION BULLETIN SBOA034 ( Comparison of Noise Performance of FET Transimpedence Amp/Switched Integrator from Bonnie Baker).
For the bandwidth optimised…
Hi Joseph,
I suggest you try and get your AFC2101 circuit to simulate correctly with the recommended supplies and GND pin at ground, before attempting the 10 V virtual ground arrangement. I suspect that if GND is offset positively by +10 V than anything…
Part Number: ACF2101
Hello,
I have some questions on some of the specifications of the ACF2101 that I could not find in the datasheet.
What is HBM/CDM (ESD) rating for this part?
Need recommended solder profile for this part.
Need to know…
Part Number: ACF2101 Hello,
I have some questions about ACF2101 that I must use in my project for studies that I can not find in datasheet.
1) If I want to use single channel (for example channel A) of this OP AMP what should I do with second channel…
Part Number: OPAMPEVM-SOIC Other Parts Discussed in Thread: ACF2101 , , IVC102 I need to evaluate an ACF2101 switched integrator. As it's surface mount I'd like to get an evaluation board.
The ACF2101 documentation says it works with the OPAMPEVM-SOIC…
Other Parts Discussed in Thread: ACF2101 Hi, I have a use for the ACF2101 switched integrator that does not fit the datasheet usage. Instead of integrating photodiode current I am measuring charge from excess charged particles hitting a halo ring. It…
Part Number: ACF2101 What are the current measurement capabilities ? Can it can measure both positive and negative currents as long as voltage at output doesn't get saturated ?
Also, what are the voltage levels that Vdd, VEE pins (and Input pins ) can…