Part Number: MSP430FR6043 Hello,
I have a question for USS SW Library.
Regarding the algorithms APIs, it is pre-compiled code and the source code is not open. Do the customer need to use it as the binary code for their production? Or is it any way to open…
Part Number: TMS320F280049 Other Parts Discussed in Thread: TIDA-010243 , MSPM0G3507 , ADS131M08 Tool/software: Hello teams,
I am trying to build a 3 phase watt meter, based on reference design TIDA-010243, i am using a C200 f280049 mcu instead of MSPM0G3507…
Hi CSC,
I have looked at MSP430F6736 and this is an e-meter SoC. This can be replaced with a 2 chip solution using our ADS131M0x and MSPM0. That would be a cost effective solution in place of the MSP430F6736. One example of the 2 chip solution is TIDA…
Hi Song,
Sorry for the late response, I got some feedback here.
The first thing to state is that:
we have now moved to SDK-based version of ADC library, just check the latest MSPM0 SDK under nortos/G3507. The code has been restructured for better portability…
Hi,
I have questions about the _USS_Algorithms_Results_ structure definition parameters,
Does volumeFlowRate refer to flow rate or flow volume?
Kind regards,
Tim
Part Number: TMS320F28388D Other Parts Discussed in Thread: C2000WARE Hello everyone, I would like to use the SPI-Interface in high-speed mode. I want to talk to two different Devices. So I need two ChipSelects. I can control those via GPIOs before the SPI…
Hi Alex,
Unfortunately we do not have an example code for this ADC, however please let me know if you have any question about it.
We do not have a metering reference design for ADS8588, but we do have more reference designs for polyphase metering based…
Hi Krunal,
Here's a a video on the Anti-aliasing filter - https://www.ti.com/video/5831231183001 the RC values are dependent on your sampling speed and input signal.
You can add a DC bias to the circuit in order to lift the signal into the acceptable…
Hi Harun,
First, congratulations that you resolved the excessive Vout issue under no load.
Regarding the snubber, as shown in your scope pictures, I do not think you really need the RC snubber on the primary side, because the circuit performance is already…
Part Number: CC2651R3SIPA Tool/software: Hello.
I'd like to know Auto-caribration for 32kHz RCOSC
Document "Running Bluetooth® Low Energy on CC13x2/CC26xx Without a 32 kHz Crystal"
descript the below.
"Refer to the BLE5-Stack Users…