Part Number: ADC128S102QML-SP Other Parts Discussed in Thread: INA213-Q1 Hello TI engineer,
In one of our projects, we are using the TI ADC chip ADC128S102QML to read the analog signal from the TI current‑monitoring chip INA213BQDCKRQ1 , which is used…
Part Number: ADC-RTD-CONFIG-CALC Other Parts Discussed in Thread: TINA-TI Hello guys,
I am designing a signal conditioning circuit for RTD ( PT100 sensor)
I designed the circuit and got DC analysis graph Voltage vs resistance as linear
I want a…
Part Number: ADS8354 In addition, For Both Channel A and B
Reference = 2.52V, input = 1.29V
Both circuits are identical (please refer to ADS8354 schematics
ADC read frequency is 500ms.
CFR REg is set to = 0x8600 - Single SDO mode 32 clocks, FSR…
Part Number: F29H859TU-Q1 We are using ADC-A only as an A/D converter and not as a comparator input.
In our development unit, a high-frequency signal is present on the ADC-A A1 input.
When the level of this high-frequency signal increases, the measured…
Part Number: TDA4VE-Q1 Team, asking on behalf of a customer:
According to the datasheet input impedance of the ADC converter changes along with sampling clock.
Could you tell me if FSMPL_CLK is fixed (60MHz) or can be modified?
Too high input…
Part Number: DRA829J Other Parts Discussed in Thread: DRA829 , Hello,
I am using the ADC module on the DRA829 processor. In my application, the analog input signals to the ADC become active before the DRA829 is powered on.
My circuit design is as…
Thanks, Tino
Because of only GPIO_4 & GPIO_5 support ADC GPIO input for TPS6522312
Few questions,
(1) if customer wants to use ADC input w/ PMIC, they should change their PDN design, isn't?
(2) Possible PDN design w/ ADC input should be PDN-7A…
Hey Gabriel,
I wanted to follow up on the ADC configuration issue you reported 29 days ago. I provided a detailed analysis focusing on two primary root causes:
DMA timing issue - Setting ADCCTL1.TDMAEN = 1 to ensure the DMA reads the result…
Part Number: ADC34RF72EVM Other Parts Discussed in Thread: LMK04828 Hello,
I have two questions regarding the ADC34RF72EVM .
The user guide (SLVUDB9) states that the ADC clock input at J5 should be driven at 9 dBm .
If the input clock power…
Part Number: PCM1822 Other Parts Discussed in Thread: PCM1841-Q1 , LM317 Dear TI-Team,
we have designed a product with (among others) a PCM1822, and most of the time it is working as expected.
However, on rare occasions (usually after running the…