Part Number: 66AK2G12 Other Parts Discussed in Thread: ADS6142 Hi,
Today we use analog converted ADS6142 and the DSP TMS320C6746EZCEA3.
The ADC is sampling 10Mhz signal and have parallel output. The DSP has uPP block which is parallel port that fits the…
Other Parts Discussed in Thread: UCC27517 Team, Can you please help with the following? Do we have some Logic or voltage translator that can support this? We have built a discrete, single-ended line transmitter in a project with the following properties: …
Part Number: DS50PCI402 I think i understand how this part works in general, i'll make some statements, please tell me where i'm wrong, or there is some nuance which i should consider.
the DEMx[1:0] pins control the Vod and De-emphasis, which…
Hi Rob,
I tried to change the system language to English, but the issue persisted. I have another ADC, which is ADS5400-sp, but it encountered the same problem of downloading FW.
Thanks,
Jie-Ming, Li
Part Number: TMS320F28379D Other Parts Discussed in Thread: SYSCONFIG Hi,
I am using the 28379D MCU
and configuring the ADC on CPU2 using sysconfig.
However, I am getting the following warning message when I try to add the ADC to CPU2.
"The ANALOG PinMux…
Part Number: MSPM0C1104 hi, experts:
We used CCS Theia 1.3.1 to configure and generate code, as known in datasheet, mspm0c1104 has a ADC with up to 10 external channels, but I've no idea how to set the channels over 4 channels in CCS Theia, it seems…
yen mei goh said: o currently the TI SPI driver does not support that? We need to modify the TI driver to support that?
The current McSPI Kernel driver only manages the CS signals in software. If you need tighter control either the driver needs to get…
Part Number: MSPM0C1104 Other Parts Discussed in Thread: MSPM0G3507 , SYSCONFIG hi, experts:
We used CCS Theia 1.3.1 to configure and generate code, as known in datasheet, mspm0c1104 has a ADC with up to 10 external channels, but I've no idea how to set…
Part Number: AFE7920
i'm bringup afe7920 with xilinx zynqmp.
In latte, we got the settings we wanted and ZYNQMP wrote the settings to the AFE7920 via SPI. But the data coming from the AFE7920 to the FPGA is unchanged.
So I wanted to send something…