Hi jlin
I have a few other comments related to the ADC operation and usage.
Since you will be using this converter in DES (Dual Edge Sampling) mode please note that you must return the device to non-DES mode whenever an on-command calibration is required…
Other Parts Discussed in Thread: TPS74401 , ADC08D1020 Hello,
I am working with the TPS74401 using a 1nF soft-start capacitor and my application is senstive to transients during start up. I have also placed some output capacitance on these LDOs to…
Hi Dan
I copied over the newest question from the other posting:
" >>> One last question for six inputs. Lets say I wanted reduce the sampling rate to 500 MSPS, use the ADC08500 as a drop in replacement. Could I then just use the SDR mode at 250 MHz…
Hi,Hooman
Thanks for your reply.
The load of the LMH6552 is ADC08D1020 and the input is differential.
I test the differential output use a single ended probe by connecting the Gnd of the probe to Vin- and another terminal to Vin+.
In addition…
Hi Reza
The DCLK_RST feature will function with an asynchronous input, but because setup and hold is not guaranteed there will be +/- 1 ADC clock uncertainty for the capture of DCLK_RST into each ADC.
To ensure all ADCs capture DCLK_RST on the same…
Hi David
Sorry about the delay responding. The LMK01020 (LVPECL outputs) can provide 1:4 distribution of the LMX2541 output at 1.5 GHz. Another option would be using the LMK04808 operating at 3 GHz internally dividing down to 1.5 GHz for 4 outputs.…
Part Number: LDC1612
I have LDC1612- H coil
I want to repeat the process of finding L,Rs, Q, C values
And Plot the Graphs for L ,Q , Rs,C Vs Frequency
I know the formula for quality factors = Rp* square root of (C/L)
How to calculate Rp?
How…
Hi All,
I want to design a WiFi operated Smart LED Bulb with Standard AC input and Also need to control dimming via micro controller as well as will drive WiFi module also.
Can anyone suggest me any solution for these requirement.
Can you suggest…