Part Number: ADC121C027 I am using the SOT package without alarm and an address line, ADR0.
I am unable to receive anything other than 0xFF when reading register 0.
I suspect it is simply not converting and FF is the POR value.
The I2C transaction…
Other Parts Discussed in Thread: ADC121C027 i have a couple of adc121c027cimk/nopb and the corresponding data sheet.
however, i can't find any pin 1 index or orientation marking on the tsot package.
does anyone know how to identify pin 1 on this…
Part Number: ADS7924 Other Parts Discussed in Thread: ADC121C027 , Hi,
We use ADS7924 and ADC121C027 on the one I2C bus, and we note that the rise time is 360ns and the high-level
hold time is 540ns. This does not meet the timing requirements of the…
Part Number: REF5050 Other Parts Discussed in Thread: ADC121C027 Tool/software: Dears,
The customer wants to select REF5050 in his new project. The customer wants to confirm whether REF5050 can also power the chip as a reference source? For example…
Part Number: ADS7924 Other Parts Discussed in Thread: OPA325 , ADC121C027 Tool/software: I am using I²C at 100kHz to read ADC data. There are two ADC chips on the I²C bus: one is ADS121C, and the other is ADS7924.
I am reading data from both ADCs in…
Part Number: INA819 Other Parts Discussed in Thread: ADC121C027 , , INA826 , INA823 , LM2776 , INA818 Tool/software: Hello,
I'm designing a circuit to amplify the signal from a electrode sensor, which presents two signals from a pair of electrodes in…
Good to hear. The reason this is an issue is that people occasionally prototype their I2C masters in host software, potentially several controllers upstream of the slave. Normally this saves development time, but it does result in slow bus transactions…