Part Number: ADC3221 Hi,
Could you recommend proper device for below requirement?
I found the ADC3221 but it can't communicate with C2000 for data.
>25MSPS
12bit
2ch
Thanks.
Other Parts Discussed in Thread: ADC3242 , ADC3241 , ADC3222 , ADC3221 Hello E2E, Please let me know how much their INL and DNL. I could not find them from datasheet.
Regards, ACGUY
Part Number: ADC3221EVM I am evaluating ADC3221 with ADC3221EVM and TSW1400.
Input clock to ADC3221 is from signal generator, sine wave, Vpp 1V.
When Input clock frequency > 22.53 MHz, the setup works. Although there are many strange spikes:
When lower…
Part Number: TSW1400EVM Default ADC3221EVM setting works with TSW1400, however, when I change ADC3221 to use 1-wire mode, this "frame clock error" pops up.
Is only default setting supported by TSW1400?
Part Number: AWR2944 Other Parts Discussed in Thread: ADC3221 , ADC3421
Our Radar have to use 24GHz band, and TI's Radar chip all moved to 60/77 GHz band. So, we have to design our own radar, with functionality and processing power similar to AWR2944…
Thank you. I will use only one ADC3221, sampling rate at 25 MHz.
Other than ADC, a MCU need a clock, although MCU can use external crystal, it's preferable if MCU also source from the same low-jitter-clock for better synchronization. The MCU accept external…
Part Number: THS4541 Other Parts Discussed in Thread: ADC3221 Hello,
I am using the ths4541 to interface to the adc3221 as described in rev C of the ADC32XXEVM schematic and very similarly, figure 80 in the datasheet. I have two configurations that are…
Part Number: THS4551 Other Parts Discussed in Thread: ADC3221 , Hi Ti.
I'm confusing, why output voltage isn't match my calculation.
Please show my schematic.
This schematic is single-end input to differential output for ADC3221.
So VOCM voltage…
Kwoki,
Without knowing much else about your application other than what you mentioned, the ADS4142 or ADS4145 would be a good choice. Another option is the ADC3221 device or one of the others in this family of parts. This is a newer part than the ADS4142…
Other Parts Discussed in Thread: DDC2256A , DDC316 , ADC3221 , ADS8168 Hi TI
Is there any digital DDC thip or ADC chip with Integrated DDC for 200K-400Khz using now?