Part Number: ADC3562 I could not find any information in the datasheet's layout section regarding whether the GND and IOGND terminals should be separated. While the documentation recommends separating the 1.8 V power supply, the application diagrams show…
Part Number: ADC3562 Other Parts Discussed in Thread: ADC3664 This is a question regarding the E-fuse loading of the ADC3562. In the thread "ADC3562: Propagation delay: the sampling clock falling edge to DCLK rising edge," Luke Allen-san commented, "0x13…
Part Number: ADC3562 Other Parts Discussed in Thread: ADC3662 ,
Tool/software:
Hi,
Could you let me confirm my register setting to work on the following setups?
Bypass mode (no decimation)
PDN/SYNC pin is used as PDN function. However, the…
Part Number: ADC3562
Hi,
The actual measured value is larger than the tPD value specified in the data sheet. Is this actual measured value acceptable for the product specification?
Also, compared to the timing chart in the data sheet, the actual…
Part Number: ADC3562 Tool/software: Hi,
The datasheet of ADC3562 shows the formula to calculate tPD as shown in below.
I think the formula should be
tPD = 3 + tCDCLK + TDCLK/2 (tCDCLK >= 2.5ns)
tPD = 3 + TDCLK + tCDCLK + TDCLK/2 (tCDCLK…
Part Number: ADC3562 Tool/software: Hi
The datasheet of ADC3562 shows thedifferential input voltage(Vid)
I think Vid is LVDS interface of electrical characteristics.
But usually, the electrical characteristics of the LVDS interface of Vid is…
Part Number: ADC3562 Other Parts Discussed in Thread: ADC3662 , , ADC3664 , ADC3664EVM Tool/software: Hi,
tPD is described in the datasheet as follows:
However, the behavior of our prototype board appears to differ from the specifications.
Since…
Part Number: THS4561 Other Parts Discussed in Thread: ADC3562 , ADC3662 , THS4541 , Tool/software: Hi,
Could you provide the best FDA for ADC3562 to meet the following conditions?
The power supply voltage for FDA is 5V. The FDA converts single-end…
Part Number: ADC3562 Other Parts Discussed in Thread: THS4541 Tool/software: Hi
This is a question about the effect of reverse leakage current of the external overvoltage protection diode of the AINP/M line.
On the 6th line of page 5 of the datasheet…
Part Number: ADC3562 Tool/software: Hi,
The datasheet of ADC3562 show the following timing chart in "8.5.2 Configuration using the SPI interface".
Where, the figure shows that SCLK is low before starting a serial packet on SPI with activating SEN…