Part Number: ADS1147 Other Parts Discussed in Thread: ADS1148 , ADS124S08 , ADS1247 , ADS1248 , ADS114S08 Hi Team,
From datasheet I found that positive/negative input of ADS1147 must be IN1~IN4, thus I doubt that this device can`t support 4 independent single…
Part Number: ADS1147
i'm a beginner .For my project i'm using ADS1147 (20PIN) . I connected the VREFOUT to VREFCOM with a 10uF capacitor. The REFPO and REFNO is not connected.
AVDD and DVDD are connected to 3.3V . The DGND and AVSS connected…
Part Number: ADS1147 Other Parts Discussed in Thread: ADS1148 I am using an ADS1147 in a design where I am measuring up to two temperature sensors (PT100, J T/C, or K T/C) and I need to measure the internal temperature for thermocouple cold junction.…
Hi James Kiely,
The pin capacitance for this family of devices (ADS1146, ADS1147, ADS1148, ADS1246, ADS1247, and ADS1248) is captured in the IBIS model: https://www.ti.com/lit/zip/sbam010
-Bryan
Part Number: ADS1147 Hi,
Could you provide sample code for ADS1147?
There is sample code in website but it's complex to the customer.
If you have more simple code for reading AIN0 through SPI with default setting, please provide it.
Thanks.
Part Number: ADS1147 Other Parts Discussed in Thread: ADS1100 Hello
i have ADS1147 and i need to set up a program in arduino whoch will be measuring AC voltage?
Does exist any libraly for that or example which i can use. This device which i am building…
Part Number: ADS1147
Hi,
I am a beginner and is involved in a board testing and I came across the ADS1147 IC (ADC with PGA-20 pin) where the REFP0 and REFN0 are not connected, instead the VREFOUT is connected to ground through a 10 uF capacitor.( from…
Hi Joseph,
I have just finished verification of the ADS1147 on my target board.
All indications are supporting the theory that the gain error when changing to PGA=8 is causing most of the system error.
I think I can address it by calibrating each unit…
Part Number: ADS112C04 Other Parts Discussed in Thread: ADS1147 Hi team,
We have a question about the ADS112C04:
Could ADS112C04 be used for two channels RTDs.
In the datasheet, the typical application is just for 1 channel RTD.
If we want to use 1 chip…
Part Number: ADS1147 Other Parts Discussed in Thread: TPD2E1B06 Tool/software: Linux Hi,
Right now I try to evaluate the ADS1147, but I cannot find a application for ESD, Burst or Surge.
I am specially interessted in the 3 Wire Ratiometric RTD Measurement…