Other Parts Discussed in Thread: ADS1224 Hi Bob
I really appreciate your help.
There is another question:
Q: Under what condition or application would you recommend enabling the buffer inside ADS1224?
I do understand the enabled buffer will increase…
Part Number: ADS1224 Hi team
My customer wants to know how well the frequency response near 50Hz and 60Hz if using the 870kHz fCLK? Datasheet only display the response curve with fCLK = 910kHz in figure 22.
Due to the accuracy issue, my customer can…
Part Number: ADS1224 Other Parts Discussed in Thread: ADS1220 , ADS1226 Hi
Our customer simulated the transmission-line model with IBIS model(ads1224.ibis: Ver 3.2). {ADS1224 ~ Line ~ MCU}
However the "drdy_dout_5" does not output.(It means the output…
Hi Steven,
Many of our Delta-Sigma converters have variable decimation/data rates and noise tables are developed and placed in the datasheets. For this device it was done differently. Generally what is seen is the noise get worse as you approach full…
Other Parts Discussed in Thread: ADS1224 , MSP430F5438A , TUSB3410 , OPA350 Hello
I am looking for a sample code which explains me the SPI interface between MSP430F5438a and ADS1224. .
It would be great if you could attach some working files.
Other Parts Discussed in Thread: ADS1224 , HALCOGEN Hi
I have to interface ADS1224 with RM48l90pge
I think to do this with spi2 pins which are sclk and somi pins for communication and cs0 and cs1 for mux controlling (behaves as IO pins)
to recive…
Jijo, It always helps to plot the communications with the ADC with an oscilloscope. On page 20 of the ADS1224 datasheet, Figure 33 shows a summary of the serial interface waveforms. You should try to duplicate those on a scope plot. If you can, plot them…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: ADS1224 , , INA233 , INA223 , ENERGYTRACE Hi, thanks for coming help!
I am looking for a solution to measure energy of low power embedded systems, including MSP430 mcus.
I know about ETT,…
Hi Andy,
I would recommend that you use the CC2541 MiniDK for both. It comes with a programmer, has a good number of break-out pins and basic auxillary functionality like buttons and LED.
If you need the high resolution, I would continue to use the…
Takumi-san,
You are correct that the ADS1251 does not have calibration. The ADS1251 was designed before we started adding calibration features and commands to our devices. Note that the ADS1251 does not have a command set or registers and is a functionally…