Other Parts Discussed in Thread: ADS1231
I designed and manufactured a weight module with ADS1231 IC and it's not working. I think I put a wrong capacitor (C7, part number: 04023C104KAT2A) in-between CAP pins. Also the capacitors between AINP1 and…
Part Number: ADS1231 Other Parts Discussed in Thread: MSP430F449 , Tool/software: I am using the ADS1231 EVM refernce board for data acquisition through DOUT & SCLK Test points mentioned in the EVM board. The test points are mentioned in the red cicles…
Part Number: ADS1231 Tool/software: Hello,
We are using ADS1231 in our product.
We are unable to find Zero drift parameter in datasheet of ASD1231. Please help for it.
If any related application note for Zero drift calculations is available please share…
Part Number: ADS1231 Tool/software: hi sir
we would like to cost down the AD7780,
Did the ADS1231 is the best solution to replace ADI/AD7780?
If yes, did you have compare table?
Thanks
Other Parts Discussed in Thread: INA823 , INA826 , ADS1231 Tool/software:
Hello,
For a load cell front end, I need an instrumentation amplifier just in front of the ADS131 ADC (24 bit, AVdd=DVdd=3.3V).
The load cell will be driven by 12V DC, has an internal…
Part Number: ADS1231 Other Parts Discussed in Thread: ADS1230 , ADS1232 , ADS1220 Hi,
How to change the gain of the internal amplifier present in the ADS1231.
Part Number: ADS1231 Other Parts Discussed in Thread: ADS1235 Tool/software: Hi,
We are using ADS1231 to interface for six wire configuration loadcell. Where excitation voltage and reference voltage is same (5V).
We have below query related to ADC behavior…
Part Number: ADS1231 hi team,
my customer wants to choose a ADC used in weighing module.They need 24bit resolution with integrated PGA.
Do u have better product to recommend except ADS1231? Thanks!
Part Number: ADS1231 Other Parts Discussed in Thread: ADS1100 , Hello,
I have an application where I was using an ADS1100 to interface a microcontroller to a full bridge. It is simple and worked great but two main things made me look for a change :
8x…
Part Number: ADS1231
Circuit Description - MCU_ADC_DOUT, MCU_ADC_SCLK is connected to MCU end, and ADC_DOUT, ADC_SCLK is connected to ADS1231 end.
Doubt 1 - I am not getting Data value in DOUT pin. Initially I have configured MCU_ADC_DOUT pin as a GPIO…