Bryan,
Thank you for the quick response.
Regarding the Vref, I apologize, but I'm a bit confused by your response. Based on the MIN, TYP, and MAX columns of the data sheet: If I plug in AVDD = 5.0V, AVSS = 0.0V to the equation and follow algebraic…
Steven,
Thanks for the details.
In the design I have used ADS1259-Q1. the main part of the program includes the data acquisition from analog world to the ADS1259-Q1, for this I would suggest please go through the ADC code snippets in the below links…
Hi, Chris,
One more question about the ADS1259EVM. From the user guide, “ to use the ADS1259EVM-PDK with the ADCPro software, the PGA280 must be used as the control for the ADS1259.”
If I'd like to bypass the PGA280, how can I record the ADS1259…
Part Number: ADS1259 Other Parts Discussed in Thread: , ADS1262 , TIPD188 Hi team,
My customer has designed in the ADS1259 to their system, and just ordered their first protoboards. As a part of the initial evaluation, they would like to be able to…
Kim,
You might be able to use something like a PGA280 in front to give you some added range (most 24-bit ADCs operate from 0 to 5V or ±2.5V. The PGA280 does operate off of ±15V supplies and is used as a a front-end for ADCs.
If you're interested…
Hi Fabien,
Welcome to the TI E2E Forums!
To use the ADS1259EVM-PDK, please make sure you are using ADCPro version 2.0.1. I recommend using the following download link: "ftp://ftp.ti.com/pub/data_acquisition/ADCPro2/no_internet_version/adcpro-wlvrt…
Other Parts Discussed in Thread: ADS1259 , PGA280 , ADS1259EVM-PDK Hi,
For mains line voltage (230V/50Hz) measurement the differential amplifier (attenuation about 115, resistors 4M4 and 38k) is used and the single-ended signal from its output is…
Hi Paul,
In order to evaluate the functionality of the PGA280 using software, you would require the ADS1259EVM-PDK. The PDK version includes the MMB0 board which serves as an interface to a computer running the EVM software. The ADS1259EVM-PDK software…
Hi David,
Did you attach a document or question to this post? If you are looking for the ADS1259 evaluation module software, you can find it here:
http://www.ti.com/tool/ads1259evm-pdk
Other Parts Discussed in Thread: ADS1259 , PGA280 , ADS1259EVM-PDK Hello all,
In need some help about power consumption using PGA280 and ADS1259. Datasheet is not so clear about this topic, only providing quiescent current.
I'm using:
VSP = …