Part Number: ADS1292 Other Parts Discussed in Thread: ADS1293 , , ADS1294R I have a system that uses the ads1293 and it works well. I want to add respiration so I want to
run a 1292R chip in sync with the 1293..
I this possible ? is it a good idea…
Tool/software:
In the ADS129x family, a 4-bit DAC is used to set the lead-off detection threshold for the positive and negative channels inputs. The DAC settings are configured writing to COMP_TH[2:0] in the LOFF control register. The threshold voltages…
Part Number: XTR110 Other Parts Discussed in Thread: AFE4900 , ADS1294R , ADS1298 Hello,
I'm measuring ECG signals. Is it possible to use loop-powered ICs (4-20mA transmitter) with the aim of lowering ECG output noise? Is it safe for body as its current…
Hi,
Additional FYI, datasheet page 65
"
(1) CH5SET and CH6SET are not available for the ADS1294 and ADS1294R. CH7SET and CH8SET registers are not available for the ADS1294, ADS1294R, ADS1296, and ADS1296R.
"
Thanks
Other Parts Discussed in Thread: AFE4960 , ADS1291 , ADS1294R Hi,
We are looking for ECG Analog front end which can be used as Single channel(As a ECG Patch) as well as Multi-Channel(As a Holter monitor).
Please suggest the best suitable AFE for our…
Other Parts Discussed in Thread: ADS1294R , ADS1298 , TPS7A89 , TPS7A87 , TPS7A88 Dear Alex, Thank you very much for your continuous support. What is the possible input for CLCKSEL, RLDIN, RLDREF pins?? If on the RLDINV pin of say ADS1294R is shorted…
Dear Alex,
To make my previous question a little bit more clear: I am planning to combine ADS1298 and ADS1294R. Use channel I of the ADS1294R for respiration and short out the rest of the channels.
I realized that the data is like 3 bytes status …
Part Number: TIPD111 Other Parts Discussed in Thread: ADS1294R , OPA348
Hello,
I did the Pace detection as mentionned in the TIPD111. Instead of 5V, I supplied the circuit to 3.3V.
This circuit is connected the PACE_OUT ADS1294R chipset.
I attached…
Part Number: ADS1298 Other Parts Discussed in Thread: TINA-TI , ADS1294R , Tool/software: TINA-TI or Spice Models Hello,
I have tried to finize the my design on ADS1298/ADS1294R; I have two questions though.
1. Is it necessary to pull up the the…
Other Parts Discussed in Thread: ADS1294 , ADS1294R , ADS1298 , ADS1299 , ADS1296 , ADS1296R , ADS1298R Hi, my name is Sang Rae Lee worked for PANAXTOS of Korea.
Our company has produced EEG product.
We are preparing new product together with one…