Part Number: ADS131M03-Q1 Other Parts Discussed in Thread: ADS131M03 Tool/software: Hi team,
Customer have inquiry on the Global-chop mode.
If using Global-Chop Mode, it will measure three sampling (n), three sampling (n+1), three sampling (n+2) times…
Part Number: ADS131M03-Q1 Tool/software: the idea is to provide exact number of clocks for a conversion to happen and then later get the result over SPI. Does it possible? thank you
Part Number: ADS131M03-Q1 Other Parts Discussed in Thread: ADS131M03 , INA236
Dear Community,
We are currently in the process of developing an ultra-low-cost current monitor specifically designed for Micro and Small Industry owners in India. Our goal…
Part Number: ADS131M03-Q1 Hi team,
I'm FAE Jimmy located in TW. My customer meet a problem that burn in time is too long. based on the diagram will need around 200hr.
Would you have any suggestion for this situation? if OK please provide the original…
Part Number: ADS131M03-Q1 Hello,
The datasheet states “Connect either SYNC/RESET or DRDY to the MCU to ensure the MCU stays synchronized to ADC conversions.”
Figure 9-2 shows them connected to GPIO on the MCU.
But also says you can use the CLKIN…
Part Number: ADS131M03-Q1 Looking at Table 8-1 in the datasheet,
If we have input 0 to 0.5V:
the max we could use would be gain of 2 and ±600 = 1200 = 2^24 so our input would be 0 to 6,990,506.7 bits?
Part Number: ADS131M03-Q1 If we supply 3.3V
Table 8-1 implies for a gain of 1, the maximum voltage that can be read is 1.2V
Customer Support told us that was for differential and to use absolute (from Table 3) would allow maximum 3.3V and to get absolute…
Part Number: ADS131M03-Q1 Other Parts Discussed in Thread: TMS320F2800156-Q1 Can you tell me the function of the CAP pin and if I can leave it floating?
The datasheet states to connect a 220nF capacitor between it and ground. The demo board (for the…
Part Number: ADS131M03-Q1
Hello all, Can someone from the community direct me to a reference design with a robust design approach for the attenuating the input voltage range of Unipolar & Bipolar 12V, 5V, 3.3V into +/-1.2V for the ADS131M03-Q1? I
Part Number: TMS320F2800157-Q1 Other Parts Discussed in Thread: ADS131M03-Q1 , C2000WARE what frequencies are available for to supply a clock for an ADC
we would like to clock the ADS131M03-Q1 as fast as possible using the TMS320F280015 6 -Q1
From…