Part Number: ADS1602 Other Parts Discussed in Thread: ADS1601 , ADS1606 , ADS1605 , ADS1625 , ADS1626 What are recommended reference options for the ADS1601, ADS1602, ADS1605, ADS1606, ADS1625, and ADS1626 devices?
Part Number: ADS1602 According to the following link, I know there's NO ADS1602 EVM.
ADS1601: Is there EVM or reference design of ADS1601 chip? - Data converters forum - Data converters - TI E2E support forums
According to the following link(slau147…
Part Number: ADS1602 Hi
I use ADS1602 to translate voltage to numerical value.
I use external vref, Vrefp=4V, Vrefn=1V, Vmid=2.5V, so I know my input can be differential Vin=3V.
But I read data, when Vin=0.5V, the numerical value=230xx(2V), Vin=0.3V…
Part Number: ADS1602 Hi team,
My customer has some question would like to ask, please see below questions.
1.) It is recommended to use OSC for CLK input, and if there are multiple ADS1602s, the CLK should be connected to each IC in parallel. Does this…
Part Number: ADS1602 Hello, I would like to know the thermal resistance of ADS1602IPFBT. ・ From junction to case temperature ・ Ambient temperature from the junction Thanking you in advance
Part Number: ADS1602 Other Parts Discussed in Thread: THS4551 ,
Hi,
We found that no matter how we change analog input, the digital output stuck at 24576 all the time.
We set /REFEN low to use internal reference, but we found that reference voltage values…
Part Number: PGA855 Tool/software: I use the PGA855 as a driver for the ADS1602. I come with a single ended signal (Vpp 0-15V) at an offset of 7.5V.
How do I connect the PGA855 correctly at the input if the input stage is powered by a single supply …
Part Number: ADS1602 Other Parts Discussed in Thread: REF5050 Hi Team,
A customer wants to know the accuracy of the internal voltage reference of ADS1602. The value of internal voltage reference at page 4 of the datasheet are min = 2.75V, typical = 3V…