Part Number: ADS4142 Other Parts Discussed in Thread: SN65LVDS9638 , LMK6D , , TSW1418EVM Hello TI Team,
I am designing a system using a high-speed pipeline ADC with the following conditions:
ADC analog supply: 1.8 V
ADC digital output:…
Part Number: ADS4142 Hello,
For several days, we observed spectral degradation only during cold starts, which disappeared after implementing the Reset assertion approximately 1 second after power-up.
Does Reset affect internal clock/timing calibration…
Part Number: ADS4142 Other Parts Discussed in Thread: CDCE72010 , LMK04228 , CDCLVP1102 Hello,
I am planning to use the ADS4142 to read in my analog signal. For this ADC, a clock driver is required in order to get the low jitter + low noise for high…
Part Number: ADS4142 Other Parts Discussed in Thread: TEST2 , Hi, I'm trying to understand the circuit around Clk input. I see it allows for differential signals between CLKN and CLKP, and the circuit for a differential sinewave clock simply inputs into…
Part Number: ADS4142 Other Parts Discussed in Thread: ADS4145 , , ADC3221 Hello,
Currently, I am searching for an ADC which can read a sine wave signal with a maximum frequency of 10 MHz. I know that I have to choose an ADC of at least 20 MHz due to…
Nidhin,
Yes, but the full scale range will be limited by half when only driving the analog inputs of the converter single ended instead of differential. The recommended max voltage would be 1.5V. This input should swing no more than VCM + 0.5V to VCM…
Part Number: ADS4145 Other Parts Discussed in Thread: ADS4142 , Dear e2e support,
Today, my customer uses our ADS4142 at 50Msps.
Could you tell me what are the consequences to replace it by our ADS4145 (for availability issue), in term of hardware…
Part Number: ADS4142EVM Other Parts Discussed in Thread: ADS58B18 , ADS4142 , ADS4149 Hi, I wanted to know whether the ADS4142 and ADS58B18 are the same. And also in the HSDC PRO GUI should i enter my ADC as 4142 or 58B18 if not can i get the ini file…
Part Number: ADS4142 Hi Team, Our customer has a slight clarification on the external RCR filter applied on the ADS4142EVM. I understand that this is to minimize input sampling glitches for low frequency operations. However, there is a slight discrepancy…
Part Number: ADS4142 Hello,
Our customer use the ADS4142, with parallel CMOS mode.
The customer connect a capacitance (less than 10pF) between CLKOUTP and GND
to reduce output noise.
When the customer remove this capacitance, there are a lot of…