Part Number: ADS5401 Hi,
I'd like to use the TI ADS5401 in a schematic, but I have a question regarding the sync input. The datasheets mentions to keep them logic low to disable this pin. However, these pins are differential LVDS inputs. Do I have to…
Part Number: ADS5401 I'd like to inquire about the ADS5401's maximum output sample value expected. With the data format set to two's complement, I'd expect the possible integers represented to be from -2^(N-1) to 2^(N-1) - 1, where N is the ADC…
Other Parts Discussed in Thread: ADS5401 Hi,
My cutomer is using ADS5401. He has question about auto correction function. Could you answer me the following questions, please?
Q1: When does auto correction finish? Datasheet shows the sequence of start…
Hi,
I posted same question following thread.
e2e.ti.com/.../545215
If you have any advice from clock side, please let me know.
-------------------------
I received the following question from my customer.
Could you tell me input capacitance and equivalent…
Other Parts Discussed in Thread: ADS5401 Hi,
My customer is consider to use the ADS5401 and has a question.
Input clock amplitude is defined 2Vpp on the datasheet.
Could you show me the voltage range of the input clock?
Best Regards,
Kuramochi
Other Parts Discussed in Thread: ADS5401 Hi, My cutomer is using ADS5401. He has question about internal LVDS termination.
"8.6.11 Register Name: 3A - Address: 0x3A" in datasheet page of 32 shows about LVDS setting. We would like to know about…
Other Parts Discussed in Thread: ADS5401 , LMK04131 Hi,
I received the following question from my customer.
Could you tell me input capacitance and equivalent circuit and of CLKIN?
They are evaluating ADS5401, and the LMK04131 provides CLK by PECL.
However…
Hi,
Customer has questions about device Initialization Timing include ENABLE pin operation.
Customer drives ENABLE pin from external. It is low logic at start up.
In datasheet, Figure 2 shows Device Initialization Timing. And, At start up, Sleep mode…
Other Parts Discussed in Thread: ADS5401 , LMK04906 Hello,
I am working with the ADS5401 high-speed data converter. The nominal sampling clock provided to the ADS5401 is a 800 MHz clock generated by the TI LMK04906. The performances of the ADS with a 800…
Other Parts Discussed in Thread: ADS5401 I'd like to inquire about the ADS5401's track and hold operation. I've read the ADS5401 data sheet (SLAS946A - APRIL 2013 - REVISED JANUARY 2014), and, from the diagram on p. 24, I see that the track…