Part Number: ADS5474-SP Hello,
Does the INL characteristic stay fairly consistent for a single device? A customer wants to know if they can calibrate it out by forming a lookup table for that particular device.
Also, I see that the typical DNL is +/-0…
Part Number: ADS5474-SP Hello team,
We have a design using the ADS5474-SP clocked at 125MHz. As the datasheet is spec’d at 250MHz we are working through how this effects a lot of the timing in the system.
We understand that (assuming a 50/50 duty…
Part Number: ADS5474-SP Other Parts Discussed in Thread: ADS5463-SP , ADS5400-SP , ADS5444-SP Hello,
Can you check the characterization data for the ADS5474-SP?
One of our customers plans to running this converter at 200MSPS. However, all the current consumption…
Hi Jim,
Thank you for your reply.
I understand that there are no vendors that can satisfy customers' demands except SP device.
I'll share with the customer.
Best regards,
Shinichi
Part Number: ADS5474 Hi Team,
Just want to confirm - are there any sequencing requirements on the ADS5474 that we'd need to adhere to between the 5V (AVDD5) and 3.3V (AVDD3 & DVDD3) rails? I see that the datasheet calls out specific requirements to bring…
Hi Noel,
Thanks for reply!
The frequency we want for clocking of four ADS5474 is 400MHz. Would jitter 801.8fs result in significant performance degradation of ADS5474 if the input frequency is around 100MHz? The datasheet shows measurements for jitter up…
Part Number: ADS5474 Other Parts Discussed in Thread: TINA-TI Is there spec performance data for ADS5474 in the case of DC-input condition?
By the way, I think that ADS5474 can use 1kHz-square wave input (50% duty), is it correct?
Best regards,
Sato…
Other Parts Discussed in Thread: DAC34H84 , ADS4249 , ADS5474 Dear All
I have ordered ADS5474, ADS4249,DAC34H84.
I need reference code for above mentioned items. Kindly give me a link
and if some one have VHDL code for Xilinx FPGA then kindly share.
Best…
Hello,
Can you share the FPGA firmware for the TSW1405, I'm want to try some custom algorithms on the FPGA, I now that TI doesn't support custom firmware but it will be a good starting point to have the source code.
Best
Carlos