Other Parts Discussed in Thread: ADS41B49 , ADS62P49 , ADS5483 Hi,
Is there any reason I shouldn't use a source impedance of several hundred ohms with a TI ADC?
The TI datasheets typically show ADCs being driven from a 50ohm or 100ohm source, but…
Yinon,
Yes, using a 1:N transformer will allow you to increase the signal swing without adding noise as this is a passive device. You will need to be careful when choosing a transformer as the linearity will vary from model to model. I have attached…
Other Parts Discussed in Thread: ADS5463 , ADS5474 , ADS5400 , ADS62P49 , ADS5483 Greetings!, I have an ADS5463 connected to a TSW1200 and am trying to programmatically control the TSW1200 via the USB/UART interface. I'm using LabVIEW (the same language…
Manos,
Contact the clocking forum regarding the pll questions of the LMX device. See if the attached documents help regarding your other questions.
Regards,
Jim
2352.Clocking High Speed Data Converters - 3_17_2013.pptx 2084.ADC Basics.pdf
5466.Clocking High Speed Data Converters - 3_17_2013.pptx 4666.ADC Basics.pdf Paul,
See section 4.3 of the document titled "ADC Basics". The second document goes into much more detail if needed.
Regards,
Jim
Are there any instructions for using the ADS548xEVM with the TSW1400 host board?
The instructions that I could find were all for the obsolete 1200 board.
I managed to get things working, but I'm not sure if I did it right.
Hardware mod: Bend J13…
Hello Tansel,
The UAF42 topology does not accommodate differential operation. I suggest using a multiple-feedback (MFB) active filter which lends itself nicely to a differential input, or fully differential filter. I wrote an article for TI's AAJ some…
Thinh,
Please use the attached ADS5484EVM User's Guide and wherever it calls out the TSW1200EVM, you will be using the TSW1400EVM. The device you select when using HSDC Pro GUI will be called "ADS5481-85. Follow the other User's Guide that is attached…