Part Number: ADS54J20 In the reference schematics, we are seeing some intermediate voltage transitions to generate the needed voltage for the ADC. Any specific reason for this? Is it mandate to follow in our application circuitry? Please share your feedback…
Part Number: ADS54J20 Other Parts Discussed in Thread: ADS54J64EVM , ADC12DJ3200 , ADC12J4000 Hi team,
The input signal is very short,so i want to control the ADC sampling when received the sampling enable.How can i achieve the function on the ads54j20evm…
Part Number: ADS54J20
Tool/software: Linux
Hi Team,
Do you have Linux driver for this module?
If it's not, Could you please suggest the best approach like
1) Write kernel space ADC driver as already written some driver in "drivers/iio/adc/" directory…
Part Number: ADS54J20EVM Other Parts Discussed in Thread: ADS54J20 Hi Team,
We observed that in the ADS54J** EVK, the terminations used for the analog signals is made as shown below for INAP, INAN, INBP and INBN signals:
In the datasheet of ADS54J20…
Part Number: ADS54J20EVM Other Parts Discussed in Thread: ADS54J20 In the reference schematics, we are seeing some intermediate voltage transitions to generate the needed voltage for the DAC. Any specific reason for this? Is it mandate to follow in our…
Part Number: ADS54J20 Other Parts Discussed in Thread: ADS54J60 Hello,
It seems that these devices are quite similar.
1) Can you please confirm they're pin compatible? Drop in compatible?
If not ,what are the differences?
2) I intend to implement…
Hello,
Customer return with one more question:
''We have the TI data acquisition module TSW14J50 EVM, the TI ADC-ADS54J20 EVM card and the TSE71 EVM clock generator.We work with your "HSDCProAutomation_64Bit.dll" in order to use your software"High…
Matt,
We offer the ADS54J20, which is a 12 bit, 1Gsps ADC that uses 4 internal ADC's (interleaved). Would this part work for your application?
Regards,
Jim
Anastasios,
See if this reference design helps. It uses an ADS54J20 which is the same as the ADS54J60 only a slower speed grade.
Regards,
Jim
ZCU102_ADS54J20_8224.zip
Other Parts Discussed in Thread: ADS54J20 , LMH3401 , LMH5401 , LMH6401 , ADS54J60 Hi
I am using the ADC (ADS54J20)in my design,but the input signal driver strenth is weak,thus it need to add the differential op AMP,how do i select the op AMP and which parameters…