Other Parts Discussed in Thread: ADS5500 , THS4513 , THS4509 Hi All:
In our ADS5500 (figure44)or THS4513(figure84) datasheet showed the circuit with input polar opposite always.
I think the circuit should be workable, but it still has phase issue…
Part Number: ADS5560 Other Parts Discussed in Thread: LMH6552 , THS4509 , ADS5500
First of all, as far as I saw in the data sheet, I saw that the ads5560 works with external 1.5V. However, I could not find the 1.5V reference IC anywhere. Secondly, In…
Part Number: THS4509 Other Parts Discussed in Thread: ADS52J90 , ADS5500 Hi TI,
I want to use THS4509 as my ADC input driver.
I find one example from the EVM design of "ADS52J90"(website: ADS52J90EVM Evaluation board | TI.com ). But this ADC chip…
Hi Mochizuki,
While looking over the THS4511 datasheet in order to respond to your question, I found a potentially useful section on the applications of the THS4511. In particular, this section discusses the default common mode output of the THS4511…
Hello Mark,
I don't have any gerber files to share, but I want to chime in on what "between the supplies" means in the Application Report you have noted:
ADS5500, OPA695: PC Board Layout for Low Distortion High-Speed ADC Drivers
It means the two…
Other Parts Discussed in Thread: THS4511-SP , TINA-TI , THS4511 , ADS5500 On page 5 of the data sheet for the THS4511-SP it lists the max and min Quiescent Current. Is the Quiescent current draw the only current draw through the THS4511-SP? Is it correct…
Other Parts Discussed in Thread: DAC5687 , ADS5500
Hi,
I am starting on a design for a digital radio using the DAC5687 + TRF3702 for the transmit chain and the ADS5500 + a demodulator for the receive chain. The baseband processing will be done in…
Other Parts Discussed in Thread: DAC5687 , ADS5500 , TSW3003 , TRF370333 Hi,
I am starting on a design for a digital radio using the DAC5687 + TRF3702 for the transmit chain and the ADS5500 + a demodulator for the receive chain. The baseband processing…
Couple of quick things Akash,
1. Where is your DC bias current path for the V+ inputs to the op amps?
2. This differential I/O op amp circuit sometimes has a common mode oscillation - probably not here, but we did see that in the OPA838 decomp device…
Hi,
There was a screenshot in the test document that did not come through in copying and pasting into the posting. I am attaching the document itself. Also, back then we had a batch file that we would run that would handle the Xilinx JTAG programming…