Part Number: ADS7042 I've read the data sheet and app notes regarding high source resistance, but the examples shown are concerned with maintaining some sample rate like 10ksps. In my application I may only need to take a measurement once every few hours…
Part Number: ADS7046 Other Parts Discussed in Thread: ADS7042 We use the ADS7042 in our design. The ADS7046 seems identical except for the 3MSPS sample rate specification. Is that true. Will this part be compatible as a drop in replacement for ADS7042…
Part Number: INA193A-EP Other Parts Discussed in Thread: ADS7042 , INA193 I'm using an INA193A-EP to sense a 30mV to 100mV shunt-based voltage. INA is powered at 5V.
By adding an RC output filter to the INA, is it possible to drive a SAR ADC like ADS7042…
Part Number: ADS7042 Hi,
based on the timing diagram (attached), ADS7042 cannot provide simultanesou sampling if there are multiple used with typical SPI. Is that correct?
I am looking for an ADC with similar characteristics, such as:
10-12…
Part Number: ADS7042 Dear Sirs,
My customer asked us about the maximum input current of the AIN_P, AIN_N input pins of the ADS 7042.
Please let me know the maximum input current of the AIN_P, AIN_N input pins of the ADS7042.
Best Regards,
…
Part Number: ADS7042 Hi Team,
One of my customer consider ADS7042 for 1ch ADC. Would you provide the feedback about below questions.
Power supply scenario They consider “AVDD=3.3V, DVDD=1.8V” or “AVDD=DVDD=1.8V”. Each power supply are independent…
Part Number: ADS7042 Hi,
I was using ADS 7042 to do "Continuity test" to check whether any electrostatic diodes are missing. But While I was doing I found that the SCLK and CS0b pins are not connected (internally ) to AVDD through electrostatic diodes…
Part Number: ADS7042 I am trying to calculate the maximum sampling rate for ADS 7042 ADC. But from the data sheet if I calculate the time I am getting only 996.5ns (1/ (12.5 * 62.5 + 15 + 200 )) for one sample. This will be greater than the sampling rate…
Part Number: ADS7042 Other Parts Discussed in Thread: ADS7057 , ADS7056 Hi Team,
I read datasheet of ADS7042 but I got confused. Can I ask some question?
There are a timing diagram at Fig 1. The output data is shown as data of sample N. But I think…