Part Number: ADS7961 Hello,
I have been trying to read values from the ADS7961 using STM32f07 using SPI but all I am getting is garbage values on the SPI Receive register of the Microcontroller.
it could be because I am packing the data wrongly while…
Part Number: ADS7961-Q1 Other Parts Discussed in Thread: TMS320F28377D , ADS7961 We are using ADS7961 in manual mode interfacing with TMS320f28377D IC on SPI
To configure the ic in Manual mode 0x1000 (channal 0 selected ) value is used and i m reading individual…
Part Number: ADS7961 Dear team.
The customer are trying to use the ADS7961EVM-PDK with ADCPro . The customer downloaded ADCPro and the ADS7961 Plug-in. When they connect the ADS7961 , they see error massage like below.
I checked E2E post, e2e.ti.com/.../594593 …
Part Number: ADS7961 I refer to a post, where it was stated, that the internal ESD diodes clamp to (+VA) with a max. current of 10mA.
I just want to validated, that this also applies to the ground. I assume this, because the max. input current is also…
Part Number: ADS7961 Other Parts Discussed in Thread: , ADCPRO Hello,
I am trying to use the ADS7961EVM-PDK with ADCPro. I downloaded ADCPro and the ADS7961 Plug-in. When I connect the ADS7961 the messages read "No firmware found...downloading -> Download…
Part Number: ADS7961 Other Parts Discussed in Thread: TLC2543 , , , ADCPRO
Reissuing a percussion sound module and updating the trigger inputs. Was using a TLC2543 but need a DAC with all the same specs but min 14 channels.
Looking for the following:
…
Other Parts Discussed in Thread: ADS7961 , ADS7961EVM-PDK , ADCPRO Hi all,
Recently i get the ads7961 evm from my local distributor. My project consist of cpld acting as spi master talking to the adc. The evm is power up with 5v and 3.3v on +va and +vbd…
Other Parts Discussed in Thread: ADS7961 , ADS7958 Hello,
We have started working ads7961 on board.
on reading channel 9any channel) I always get up to 7bit scale , but no more than that.
for example:
for channel 0: 0x07E0
for channel 1: 0x17E0
for channel…
Part Number: OPA992 Other Parts Discussed in Thread: ADS7961 , , LM7705 , OPA2810 , OPA355
For our design, we have 16 channels and connect to ADS7961, as this picture:
I read here design for photodiode TIA:
https://www.ti.com/lit/pdf/tidu535
Regarding …
Hi Dewei,
don't forget the maximum negative input voltage range of ADS7961:
https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1197893/opa992-suggestion-about-provide-bias-for-tia
Kai