Hi All,
Additional inputs
Customer is asking if there is a way their firmware can tell if the CPU is AM3352 or AM554D80 or Z100? Like a register to read from?
Please refer to the below register
Data sheet reference:
www.ti.com/.../am3352.pdf
3 Device…
Part Number: AM3357 Other Parts Discussed in Thread: SYSBIOS Tool/software: Hi,
I have a need for product updates,
The original environment was
am335x_sysbios_ind_sdk_01.01.02.01
SYS/BIOS 6.41.4.54
XDC Tool 3.31.3.43
CCS 6.0
am335x_sysbios_ind_sdk_01…
Part Number: AM3357 Tool/software: Hi experts,
We have an external NOR flash (Multiplexed Address Data 16-Bit Device) that communicates properly with an AM3357 processor, as long as it is Silicon Revision 2.0 or higher.
If the processor is a Silicon…
Part Number: AM3357 Other Parts Discussed in Thread: CSD Hi,
We am trying to use THGBMJG6C1LBAU7 EMMC with the AM3357 processor on our hardware. The UBOOT is on the SPI flash and from there it is executing the linux kernel's zImage which fetches the rootfs…
Part Number: AM3357 Other Parts Discussed in Thread: AMIC110 , Hi,
Regarding the replacement of AMIC110 → AM3357, we were able to confirm normal operation with the same binary. We are planning to change the A8 core clock from 300MHz to 600MHz in the future…
Part Number: AM3357 Other Parts Discussed in Thread: AMIC110 , , TMDSEMU110-U , TMDSEMU200-U Hi,
I have a question regarding the development environment for AMIC110 and AM3357. According to TI's website, the following products are compatible with the debugger…
Part Number: PRU-ICSS-INDUSTRIAL-SW Other Parts Discussed in Thread: AM3357 In our implementation we leverage a single port (Port 0) of the RMII interface and MDIO of the AM3357 to communicate via EtherCAT through the PRU-ICSS and a DP83826 PHY. To do so…
Part Number: AM3357 Other Parts Discussed in Thread: PROFIBUS , Hi, My customer released Profibus slave product using AM3357. One of their end customers reported a communication error happens periodically. According to their investigation, the error happens…
Part Number: TMDSEMU110-U Other Parts Discussed in Thread: AM3357 , AMIC110 Hi,
We are using TMDSEMU110-U for debugging AM3357. It worked without problems when debugging AM3357 at 300MHz. However, after increasing the frequency of AM3357 to 600MHz, the…