Part Number: AM62L-EVSE-DEV-EVM We have manufactured TIDA- 010239 reference kit and procured PHYTEC-3P-AM62x for developing an AC Charger solution. Currently, we are able to run Charger in simulating environment on phytec board and followed steps like…
Part Number: AM62L-EVSE-DEV-EVM SDK 11.2 may have an issue with stack corruption due to position/alignment that was fixed in SDK 12. Is there any formal analysis for efficiency/robustness related to improvements done in SDK 12 that triggered these (and…
Tina Mary Pereira said: This is the stats while streaming uisng UDP for around 15 minutes.
The CPU load isn't high.
Tina Mary Pereira said: There is no frame jump now, but we are observing that the frame freezes for a few milliseconds , now and then…
Hi Priyanka,
priyanka shobhan said: but in issue case , 3 of these leds goes off momentarily then on and 4th one blinks.
What is the PCB silkprint label of the 4th LED?
Split from AM62L-EVSE-DEV-EVM: AM62AX-EVM-K3R5: Yocto build fails in linux-firmware:do_package with pseudo errors (Cannot mkdir: Bad address)
Hi,
This is a classic Yocto sstate/deploy-manifest desync , and given the timing, it's very likely a direct…
Hello JIE WANG,
Thank you for your query !
I have started the analysis of the issue and a discussion within my team, however:
JIE WANG said: 1. ETS Firmware Version : ets.2.46.0.2.img.xz
part number:AM65x EVM PROCESSOR BOARD PROC062B
Would you…
Hi Mariusz,
thank you for the update. If you are sure that the resistor R6 is correctly soldiered, then we should say that either the WLAN1837MOD pin 14 is NOT contacting the pad on board, or the trace is cut at some place. According to your experiments…
Hi Tina,
It seems that your storage is full.
Tina Mary Pereira said: /home/tpereira/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/qtdeclarative/6.9.2/qtdeclarative-6.9.2/src/quick/scenegraph/util/qsgvertexcolormaterial.h:21:2: fatal error…
Part Number: AM62L-EVSE-DEV-EVM Hello Team, We are working on AM62L3x based custom device, we are using SDK 11.00.15.05, we are using DP83822 ethernet phy ic in RMII mode. We have enabled secure boot on the device. Before enabling secure boot the ethernet…
Part Number: AM62L-EVSE-DEV-EVM-DOC-CERT Other Parts Discussed in Thread: AM62L Hello,
I'm a Advisor of technical marketing at FeRAM memory maker, and our customer is willing to use our QSPI based FeRAM (4M).
This customer has been using MRAM memory…