Part Number: SK-AM69
Tool/software:
Hi,
I'm working on project that requires memory allocation for DMA. While working on it, It seems like there is memory corruption on allocated memories.
So we made programs to test this.
dma_bridge.tar.gz
Each program…
Part Number: SK-AM69 Other Parts Discussed in Thread: AM68 , AM69 , SYSCONFIG , AM69A
Tool/software:
Team,
Could you please help with the below question: Config:
TI SK-AM69 unit
XDS560 V2 system trace modulator
Linux ubuntu 22.04 with CCS v20.1 + Linux…
Part Number: AM69A Other Parts Discussed in Thread: AM69 Tool/software: Hi Sir,
What is the purpose of OSPI in the AM69 EVM reference design? If it is not used in my design, can it be removed directly?
Thanks.
Gary
Update: I am following the "Installing GstShark on Yocto" from https://developer.ridgerun.com/wiki/index.php/GstShark_-_Getting_Started#Getting_the_code
Where I download meta-gstshark from https://github.com/RidgeRun/meta-ridgerun/tree/mast…
Part Number: SK-AM69
Tool/software:
Hello, Ti.
I set the MCU_SPI1_* pins as SPI Master and connected to SPI sensors to test out SPI functions.
I used spidev_test command to read sensor(ADXL345) ID (which should be 0xE0). I checked MISO line with oscilloscope…
Hi Andy,
CPSW uses the switchdev layer of linux not dsa.
Andy Nicholas said: My company would like to use the embedded networking ports on the AM69 as individual, discrete ports instead of switched-ports
But What you want is already the default configuration…
Part Number: AM69 Other Parts Discussed in Thread: TDA4VH , Tool/software: Can you share IBIS file of AM69A the part number which is below?
XAM69A98ATNGHAALY
Part Number: AM69 Tool/software: Hello TI Experts, We have custom hardware based on the AM69 SoC and intend to use the PCIE_SOC_REFCLK0_OUT, PCIE_SOC_REFCLK1_OUT, PCIE_SOC_REFCLK2_OUT, and PCIE_SOC_REFCLK3_OUT pins to provide reference clocks for PCIe…
Part Number: AM69 Tool/software: Hello,
On our custom board we will be using the internal reference clock (core_refclk) to the 4 lane SERDES.
The internal reference clock is input-muxed; we will be using the MAIN_PLL2_HSDIV4_CLKOUT (100 MHz) input to…